2013-06-24 4:25 AM
hello dear forum,
I am using eeprom emulation on my F103FLASH_Unlock();
EE_Init();
EE_ReadVariable(0x5501,&RAM[PARAMETERS]);
what I want ask is I am read protecting my F103 product before sale
doesthis Flash_Unlock() function disables read protection ? thank you #stm32f103-flash2013-06-24 5:34 AM
It is a magic sequence to enable access to the flash controller registers, to prevent errant code writes to flash, it doesn't alter Read/Write protection on the array.
2013-06-25 1:33 AM
hello,
so ... is it better to Flash_Lock() again ( to prevent errant writes ) right after I Flash_Unlock() and EE_read/EE_write ? thank you2016-01-07 1:39 AM
is it possible to upgrade firmware of stm32f103 controller remotely via OTA
2016-01-07 2:15 AM
Yes, is there a reason why you have to ask this same question in four threads?
2016-01-07 8:26 PM
hello sir,
can you please explain how to do firmware upgradation of stm32f103 via OTA2016-01-07 8:50 PM
Suggest you review the IAP (In Application Programming) examples for your part. Build yourself a small loader that uses your specific type of 'Air' to transfer the data, and erase and write blocks of flash with this new data.
2016-01-07 10:21 PM
Thanx
2016-02-14 9:25 PM
2016-02-14 10:52 PM
Yes , it is absolutely possible. Are you facing any problem in this.
/*Please
mark helpfull
if this post helps you or solves your problem.*/
/* If you need any personal support for your work pleasecontact at
embeddeddesign.help@gmail.com*/
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.