2014-07-14 3:53 AM
Hello, I like to use DMA1 in my STM32F103 application. I need 6 timer triggered channels.
So i choosed from reference manual pg. 273: Channel 1: TIM4_CH1 Channel 2: TIM3_CH3 Channel 3: TIM3_UP Channel 4: TIM4_CH2 Channel 6: TIM3_CH1 Channel 7: TIM4_UP I used the configuration of some examples. TIM3 and TIM4 are configured identical. All DMA Channels are configured and enabled the same way. But I only get request events from TIM4! (tested with ''transmission complete''-interrupt) So my question is: is it possible to use 6 Channels of one DMA? Did i missed something? thanks in advance #stm32f103-dma1-tim3-tim4-dma-tim2014-07-14 6:31 AM
Not aware of anything that would preclude the use of multiple channels.
2014-07-14 10:04 AM
Ok i tried with only one Timer:
I am using TIM1 on DMA1: Channel 2: TIM1_CH1 Channel 3: TIM1_CH2 Channel 4: TIM1_CH4 Channel 5: TIM1_UP Channel 6: TIM1_CH3 Channel 2 and 3 are not working :( the others are fine... It seemes that there are combinations which are not working together... DMA_InitTypeDef DMA_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); DMA_Cmd(DMA1_Channel1, DISABLE); DMA_Cmd(DMA1_Channel2, DISABLE); DMA_Cmd(DMA1_Channel3, DISABLE); DMA_Cmd(DMA1_Channel4, DISABLE); DMA_Cmd(DMA1_Channel5, DISABLE); DMA_Cmd(DMA1_Channel6, DISABLE); DMA_Cmd(DMA1_Channel7, DISABLE); DMA_DeInit(DMA1_Channel1); DMA_DeInit(DMA1_Channel2); DMA_DeInit(DMA1_Channel3); DMA_DeInit(DMA1_Channel4); DMA_DeInit(DMA1_Channel5); DMA_DeInit(DMA1_Channel6); DMA_DeInit(DMA1_Channel7); DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; DMA_InitStructure.DMA_BufferSize = 1; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_VeryHigh; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word; /* DMA1 Channel5 Config TIM1_UP*/ DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t) & GPIOA->BSRR; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t) & this->DmaIn[0]; DMA_Init(DMA1_Channel5, (DMA_InitTypeDef*) &DMA_InitStructure); /* DMA1 Channel2 Config TIM1_CH1*/ DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t) & GPIOB->BSRR; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t) & this->DmaEn[0]; DMA_Init(DMA1_Channel2, (DMA_InitTypeDef*) &DMA_InitStructure); /* DMA1 Channel3 Config TIM1_CH2*/ DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t) & GPIOB->BSRR; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t) & this->DmaEn[1]; DMA_Init(DMA1_Channel3, (DMA_InitTypeDef*) &DMA_InitStructure); /* DMA1 Channel6 Config TIM1_CH3*/ DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t) & GPIOA->BSRR; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t) & this->DmaIn[1]; DMA_Init(DMA1_Channel6, (DMA_InitTypeDef*) &DMA_InitStructure); /* DMA1 Channel4 Config TIM1_CH4*/ DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t) & GPIOA->BSRR; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t) & this->DmaIn[2]; DMA_Init(DMA1_Channel4, (DMA_InitTypeDef*) &DMA_InitStructure); TIM_DMACmd(this->timer1->timerReg, TIM_DMA_Update, ENABLE); TIM_DMACmd(this->timer1->timerReg, TIM_DMA_CC1, ENABLE); TIM_DMACmd(this->timer1->timerReg, TIM_DMA_CC2, ENABLE); TIM_DMACmd(this->timer1->timerReg, TIM_DMA_CC3, ENABLE); TIM_DMACmd(this->timer1->timerReg, TIM_DMA_CC4, ENABLE); DMA_Cmd(DMA1_Channel2, ENABLE); DMA_Cmd(DMA1_Channel3, ENABLE); DMA_Cmd(DMA1_Channel4, ENABLE); DMA_Cmd(DMA1_Channel5, ENABLE); DMA_Cmd(DMA1_Channel6, ENABLE);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.