2012-10-04 4:20 AM
hi all,i am recently working on a project that sending AT command to gsm module from stm32f100c8 via usart and receiving response with interrupt but i am very confused about usart interfaces.i cant receive response from gsm module.i am using stm32vl discovery and ublox leon g100 gsm module usart1 and usart3 and terminal.It sends me back same string.i send ''AT'' and i want to get ''OK'' response from module.please help where am i wrong?here is my code :
/*----------------------------------------------*/
/*----------------------------------------------*/
#include ''stm32f10x.h''
#include ''stdio.h''
#include ''string.h''
/*----------------------------------------------*/
/*---------function prototypes------------------*/
void RCC_Configuration(void);
void GPIO_Configuration(void);
void NVIC_Configuration(void);
void USART_Configuration(void);
void ResetModule(void);
void USART_SendCommand(unsigned char *s);
/*------------------------------------------------*/
/*-------------global variables-------------------*/
unsigned char command[]=''AT\0\r\n'';
char response[50];
int res_index=0;
unsigned char r;
/*----------------------------------------------*/
/*----------RCC configurations------------------*/
void RCC_Configuration(void){
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
}
/*----------------------------------------------*/
/*----------GPIO configurations------------------*/
void GPIO_Configuration(void){
GPIO_InitTypeDef GPIO_InitStructure;
/* Configuring USART1_Tx as 'alternate function push-pull' */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Configuring USART1_Rx as 'input floating' */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Configuring USART3_Tx as 'alternate function push-pull' */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Configuring USART3_Rx as 'input floating' */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* reset the module*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_Init(GPIOB, &GPIO_InitStructure );
}
/*----------------------------------------------*/
/*----------USART configurations----------------*/
void USART_Configuration(void){
USART_InitTypeDef USART_InitStructure;
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1, ENABLE);
USART_Init(USART3, &USART_InitStructure);
USART_Cmd(USART3, ENABLE);
USART_ITConfig(USART3, USART_IT_RXNE, ENABLE);
}
/*----------------------------------------------*/
/*----------NVIC configurations-----------------*/
void NVIC_Configuration(void){
NVIC_InitTypeDef NVIC_InitStructure;
NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
/*----------------------------------------------*/
/*----------RESET module-----------*/
void ResetModule(void){
long int n;
//reset
GPIO_SetBits(GPIOB,GPIO_Pin_13);
for(n = 0;n < 10000000;n++);
GPIO_ResetBits(GPIOB,GPIO_Pin_13);
for(n = 0;n < 30000000;n++);
//power
GPIO_SetBits(GPIOB,GPIO_Pin_12);
for(n = 0;n < 10000000;n++);
GPIO_ResetBits(GPIOB,GPIO_Pin_12);
}
/*----------------------------------------------*/
/*----------Main function-----------------------*/
int main(){
RCC_Configuration();
GPIO_Configuration();
USART_Configuration();
NVIC_Configuration();
ResetModule();
USART_SendCommand(command);
while(1){
}
}
/*----------------------------------------------*/
/*----------Send command------------------------*/
void USART_SendCommand(unsigned char *s)
{
while(*s)
{
//while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET);
//USART_SendData(USART1, *s);
while(USART_GetFlagStatus(USART3, USART_FLAG_TXE) == RESET);
USART_SendData(USART3, *s++);
}
}
/*----------------------------------------------*/
/*----------Receive character from USART3-------*/
void USART3_IRQHandler(void){
r=USART_ReceiveData(USART3);
response[res_index]=r;
res_index++;
}
/*----------------------------------------------*/
/*--------------------------------------------------------------------------------------------*/
/*--------------------------------------------------------------------------------------------*/
/*--------------------------------------------------------------------------------------------*/
/*--------------------------------------------------------------------------------------------*/
2012-10-05 4:24 AM
i think you mean that..not to send command in the code,send it from terminal.here is my code but the result is the same:(..
/*----------------------------------------------*//*----------------------------------------------*/#include ''stm32f10x.h''#include ''stdio.h''#include ''string.h''/*----------------------------------------------*//*---------function prototypes------------------*/void RCC_Configuration(void);void GPIO_Configuration(void);void NVIC_Configuration(void);void USART_Configuration(void);void USART3_IRQHandler(void);void USART1_IRQHandler(void);void ResetModule(void);/*-----------------------------------------------*//*-------------global variables------------------*/unsigned char r;unsigned char c;/*----------------------------------------------*//*----------RCC configurations------------------*/void RCC_Configuration(void){ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE); }/*----------------------------------------------*//*----------GPIO configurations-----------------*/void GPIO_Configuration(void){ GPIO_InitTypeDef GPIO_InitStructure; /* Configuring USART1_Tx as 'alternate function push-pull' */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configuring USART1_Rx as 'input floating' */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configuring USART3_Tx as 'alternate function push-pull' */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOB, &GPIO_InitStructure); /* Configuring USART3_Rx as 'input floating' */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOB, &GPIO_InitStructure); /* reset the module*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOB, &GPIO_InitStructure );}/*----------------------------------------------*//*----------USART configurations----------------*/void USART_Configuration(void){ USART_InitTypeDef USART_InitStructure; USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_Init(USART1, &USART_InitStructure); USART_Cmd(USART1, ENABLE); USART_Init(USART3, &USART_InitStructure); USART_Cmd(USART3, ENABLE); USART_ITConfig(USART3, USART_IT_RXNE, ENABLE); //usart3 receive interrupt USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);// usart1 receive interrupt }/*----------------------------------------------*//*----------NVIC configurations-----------------*/void NVIC_Configuration(void){ NVIC_InitTypeDef NVIC_InitStructure; NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0); NVIC_InitStructure.NVIC_IRQChannel = USART3_IRQn; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; //usart3 priority=0 NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; //usart1 priority=1 NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);}/*----------------------------------------------*//*----------RESET module------------------------*/void ResetModule(void){ long int n; //reset GPIO_SetBits(GPIOB,GPIO_Pin_13); for(n = 0;n < 10000000;n++); GPIO_ResetBits(GPIOB,GPIO_Pin_13); for(n = 0;n < 30000000;n++); //power GPIO_SetBits(GPIOB,GPIO_Pin_12); for(n = 0;n < 10000000;n++); GPIO_ResetBits(GPIOB,GPIO_Pin_12);}/*----------------------------------------------*//*----------Main function-----------------------*/int main(){ RCC_Configuration(); GPIO_Configuration(); NVIC_Configuration(); ResetModule(); USART_Configuration(); while(1){ }}//usart1 receive character from terminalvoid USART1_IRQHandler(void){ while(USART_GetFlagStatus(USART1, USART_FLAG_RXNE) == RESET); c=USART_ReceiveData(USART1); //send character to usart3 TX while(USART_GetFlagStatus(USART3, USART_FLAG_TXE) == RESET); USART_SendData(USART3, c);}/*----------------------------------------------*//*----------Receive character from USART3-------*/void USART3_IRQHandler(void){ r=USART_ReceiveData(USART3); //receive character from usart3 RX while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); //send to usart1 for display in terminal USART_SendData(USART1, r);}/*----------------------------------------------*//*-----------------------------------------------------*//*-------------------------------------------------------------*//*------------------------------------------------------------------------*//*--------------------------------------------------------------------------------------------*/2012-10-05 9:02 AM
Not the software.
You need to examine how you have the GSM module hooked up, and that it's powered up, or turned on, communicating with the SIM, etc. I would suggest you break a scope out and probe the critical pins. If the module has an evaluation board connect that to a PC and test that. Perhaps you can provide something like a schematic or circuit diagram? Remember that the STM32 USARTs operate at CMOS levels, and NOT RS232 levels.2012-10-06 1:27 AM
i think connections are true,because i took GPS sentences and parsed them with same module and mechanism,now i screw up GSM part and AT commands
2012-10-07 8:37 AM
i think connections are true,because i took GPS sentences and parsed them with same module and mechanism,now i screw up GSM part and AT commands
Great, but no one here has any concrete information to work from You need to provide much more specific detail of how you have this wired up.2012-12-12 11:50 PM
2012-12-14 10:17 AM
hi chi,
try this command,i solved the problem now i am receiving response:
AT&k0E0+IPR=115200
115200 is here baud rate
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.