2013-09-19 6:57 AM
Hi all,
I have trouble with RTC on STM32VLDISCOVERY board.After initialization, when I'm calling RTC_WaitForLastTask() after RTC_SetCounter() function, the MCU falls into an infinite loop.I can't get what is wrong.Is this hardware issue, if yes is there any workaround?My Code is :void RTC_Configuration(void)
{ /* Enable PWR and BKP clocks */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR | RCC_APB1Periph_BKP, ENABLE);/* Allow access to BKP Domain */
PWR_BackupAccessCmd(ENABLE);/* Reset Backup Domain */
BKP_DeInit();/* Enable LSE */
RCC_LSEConfig(RCC_LSE_ON); /* Wait till LSE is ready */ while (RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET);/* Select LSE as RTC Clock Source */
RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE);/* Enable RTC Clock */
RCC_RTCCLKCmd(ENABLE);/* Wait for RTC registers synchronization */
RTC_WaitForSynchro();/* Wait until last write operation on RTC registers has finished */
RTC_WaitForLastTask();/* Enable the RTC Second */
RTC_ITConfig(RTC_IT_SEC, ENABLE);/* Wait until last write operation on RTC registers has finished */
RTC_WaitForLastTask();/* Set RTC prescaler: set RTC period to 1sec */
RTC_SetPrescaler(32767); /* RTC period = RTCCLK/RTC_PR = (32.768 KHz)/(32767+1) */ /* Wait until last write operation on RTC registers has finished */ RTC_WaitForLastTask();/* Set RTC counter: set RTC counter to 0 */
RTC_SetCounter(0); /* Wait until last write operation on RTC registers has finished */ RTC_WaitForLastTask();}void main() { .... if (BKP_ReadBackupRegister(BKP_DR1) != 0xA5A5) { RTC_Configuration(); BKP_WriteBackupRegister(BKP_DR1, 0xA5A5); } else { RTC_WaitForSynchro(); RTC_ITConfig(RTC_IT_SEC, ENABLE); RTC_WaitForLastTask(); } RCC_ClearFlag(); .... while(1) { .... RTC_WaitForLastTask(); RTC_SetCounter(1379598788); RTC_WaitForLastTask(); .... }}Thanks in advance.Best Regards,Hayk #stm32f10x-rtc2013-09-19 8:00 AM
We have the synchro-command at the end of the config. Rest is equal.
2013-09-19 8:04 AM
You probably need this in else-path, too:
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR | RCC_APB1Periph_BKP, ENABLE);PWR_BackupAccessCmd(ENABLE);
I would enable IT-Config after synchro.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.