2013-09-18 2:58 AM
Hello,
I want to protect my ADCs from overvoltage and ESD, and limiting the input to 3.3V.This is my schematic:2013-09-18 6:54 AM
I use the ST USBLC6-4 series TVS diode arrays. They are intended for USB but work well as a low capacitance TVS diode. The array clamps the input line to the power rails. I like the USBLC6 since it has either 2 or 4 diodes for multiple channels plus a fast breakdown diode between ground and VDD.
For single diodes and no line clamping I use the NXP PESD series TVS diodes for 5V and 3.3V lines. For 24V outputs (common in industrial process control) I use the Vishay QSBT40 TVS diode array. I also use zeners to clip the input voltage to an ADC channel in cases where the ADC VREF is below the VDD power rail. Jack Peacock2013-09-18 8:38 AM
a Zener is too slow for transient suppression
Erik2013-09-19 7:58 AM
Thanks ! I also use the PESD5V0S1 for my resistive touchpad input. I think I will use it for my ADC inputs.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.