2013-10-31 6:44 AM
Hi all,
Ive got a bit of a problem with a bootloader. Everything is running just fine out of RAM (.text .rodata .data), but im having issues moving over the vector table. Ive reserved 0x200 bytes at the start of RAM in the linker script, then at the start of the bootloader i do:memcpy((char*)0x20000000, (char*)0x8000000, 0x1E4);
NVIC_SetVectorTable(NVIC_VectTab_RAM, 0);
Is there anything wrong with doing this?
When i do, i have a weird issue with FatFS not being able to open a file on a uSD card.
If i comment out those two lines and leave the table in flash, it works just fine.
Any ideas?
Thanks in advance!!
2013-10-31 9:43 AM
It's doesn't look offensive, moving it won't relocate what it points too.
Make sure you've carved the space out properly, review the .MAP and check it doesn't use that area of RAM. Check variables, stack, etc.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.