2013-10-31 1:04 AM
Hi, I am trying to communicate with MCP4725(12bit DAC) via I2C using STM32F030C8T6. The program gets stuck at one of the status checking part. Can somebody look at my code and see what the problem is?
//Code to Initialize I2C void InitI2C(void){ //PB8 = SCL1, PB9 = SDA1 RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);//I2C1 RCC_I2CCLKConfig(RCC_I2C1CLK_HSI); //I2C RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);//I2C1 GPIO GPIO_PinAFConfig(GPIOB, GPIO_PinSource8, GPIO_AF_1); GPIO_PinAFConfig(GPIOB, GPIO_PinSource9, GPIO_AF_1); GPIO_StructInit(&GPIO_InitStruct); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_8; //SCL GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_OType = GPIO_OType_OD; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOB, &GPIO_InitStruct); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_9; GPIO_Init(GPIOB, &GPIO_InitStruct); I2C_InitStruct.I2C_Mode = I2C_Mode_I2C;//NOt SMBUS host I2C_InitStruct.I2C_AnalogFilter = I2C_AnalogFilter_Enable; I2C_InitStruct.I2C_DigitalFilter = 0x00; I2C_InitStruct.I2C_OwnAddress1 = 0x00; I2C_InitStruct.I2C_Ack = I2C_Ack_Enable; I2C_InitStruct.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStruct.I2C_Timing = 0x10400CDB;//STM�?� I2C Configuration tool I2C_Init(I2C1, &I2C_InitStruct); I2C_Cmd(I2C1, ENABLE); } //code to communicate with I2C void WriteMCP4725(uint16_t data){ uint8_t high_buffer, low_buffer; if(data > 4095) data = 4095; high_buffer = (uint8_t)((data>>8) & 0xFF); low_buffer = (uint8_t)(data & 0xFF); while(I2C_GetFlagStatus(I2C1, I2C_ISR_BUSY) != RESET); I2C_TransferHandling(I2C1, 0xC0, 2, I2C_AutoEnd_Mode, I2C_Generate_Start_Write); //Generate Start Condition while(I2C_GetFlagStatus(I2C1, I2C_ISR_TXIS) == RESET); I2C_SendData(I2C1, high_buffer); while(I2C_GetFlagStatus(I2C1, I2C_ISR_TCR) == RESET); I2C_SendData(I2C1, low_buffer); while(I2C_GetFlagStatus(I2C1, I2C_ISR_STOPF) == RESET); I2C_ClearFlag(I2C1, I2C_ICR_STOPCF); } am i doing something wrong?? my program doesn't get past the while(I2C_GetFlagStatus(I2C1, I2C_ISR_TCR) == RESET); part Here is the code that works with PIC and CCS compiler void ext_dac_out(uint8_t dac_type, uint8_t out_sel, uint16_t dac_buffer){ int8 buffer; int8 high_buffer, low_buffer; buffer = 0b11000000;//MCP4725 high_buffer = dac_buffer>>8; low_buffer = dac_buffer; i2c_start(); i2c_write(buffer);//address byte, write mode i2c_write(high_buffer);//fast write commands(C2,C1,PD1,PD0,D11-D8) i2c_write(low_buffer); //write data(D7-D0) i2c_stop(); Thank you2013-11-19 2:08 AM
Which StandardLib version are you using?
The flag names should be ''I2C_FLAG_xxxx'' not ''I2C_ISR_xxxx'' or ''I2C_ICR_TCR''. -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.