STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L Discovery Board no target connected help

Posted on November 20, 2013 at 03:28Over the summer, I attended a STM32L seminar. I got the board to connect and program perfectly on my work laptop. Since then the board has sat in my drawer, but I just recently got out to use on a school project. ...

zlbearss by Associate
  • 1601 Views
  • 3 replies
  • 0 kudos

ADC AWD int channel

Posted on November 01, 2013 at 04:41Hi, I setted-up ADC1 to monitor 4 channels with AWD. Is it possible to know which channel caused the interupt in the ADC1_2_IRQHandler ? #stm32-adc-awd-interup

fernand by Associate
  • 1018 Views
  • 1 replies
  • 0 kudos

SPI DMA receive problem

Posted on November 18, 2013 at 14:03Hi,I am using SPI with DMA in STM32F427 for full duplex communication with another processor. My configuration for SPI and DMA is follows;       SPI_InitTypeDef SPI_InitStructure;           GPIO_InitTypeDef GPIO_I...

asecen89 by Associate II
  • 1400 Views
  • 2 replies
  • 0 kudos

STM32F103Z Timer Problem

Posted on November 18, 2013 at 17:43I have a Timer Problem . I want that my timer every 1ms makes an interrupt . I testes it here if (TIM2_Tick >= 1000) but my LED was alway on then I tryied if (TIM2_Tick >= 1000000) and it was about 1 sec (30 bli...

samed by Associate II
  • 2528 Views
  • 5 replies
  • 0 kudos

STM32F4 DCMI no line interrupt

Posted on November 07, 2013 at 21:06 Hi I've some problems with the dcmi interface from my stm32f4 I've initialized the module for line and frame interrupts, but in debug I see only the frame complete interrupt, and a line count variable...

pa by Associate II
  • 1423 Views
  • 1 replies
  • 0 kudos

ADC

Posted on November 19, 2013 at 06:06Hello ,         I am working on application in which battery voltage need to be read at regular interval say 1 ms .I am newbie to this.(1) Which one is more preferred here ADC with DMA or ADC w\o DMA ?(2) How many...

STM32F0x I2C problem

Posted on October 31, 2013 at 09:04Hi, I am trying to communicate with MCP4725(12bit DAC) via I2C using STM32F030C8T6. The program gets stuck at one of the status checking part. Can somebody look at my code and see what the problem is? //Code to Ini...

Calculation of ADC sampling rate

Posted on November 19, 2013 at 09:11Hello,♯ I am working with STM32F4 Discovery  and summon arm tool chain.I am sending ADC  data over       serial Port using USB serial communication.♯ I have write code to get ADC value in continuous conversion mod...

Mapping System clock on GPIO

Posted on November 15, 2013 at 14:06Hi all,I'm working with STM32F3DISCOVERY.I'm trying to map the system clk on a GPIO to view it with an oscilloscope.In the following datasheet http://www.st.com/st-web-ui/static/active/en/resource/technical/docume...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.