2021-03-10 2:38 AM
Hello,
I have a board that use STM32F072C8T6TR reference.
After severel weeks of normal use, the STM32 on some boards are not responding anymore. I tried to access the STM32 with STlink Probe, ore by using internal Bootlaoder, without success. After investigations, I can see that the NRST pin (which is internally pulled up, and not connected to any other component on my board) never goes high, and thus I suspect that the MCU is dead.
The STM32 only use some GPIOs for SPI communication with components that share the same VDD Power supply.
The only idea I have, is that the VDDDIO2 that power the USB PHY and some GPIOs is only powered when a USB cable is connected to my board. I understood in the datasheet that the VDD and VDDIO2 domais are completly independant, and thus the VDDIO2 can be shut off even if the STM32 is running.
Is it correct ? If not, could it explain the behaviour I have ?
Thanks,
Solved! Go to Solution.
2021-03-10 2:47 AM
Read the datasheet again: "The VDDIO2 voltage level is completely independent from VDD
or VDDA, but it must not be provided without a valid supply on VDD."
2021-03-10 2:47 AM
Read the datasheet again: "The VDDIO2 voltage level is completely independent from VDD
or VDDA, but it must not be provided without a valid supply on VDD."
2021-03-10 4:00 AM
Hi Uwe,
Thansk for your answer. I agree with you, and our design respect the datasheet :
Thus, the VDDIO2 cannot be provided without a correct VDD, in accordance to the datasheet.
2021-03-12 8:21 AM
If the source supplying VDDIO2 is capable, consider a Zener of about 3 V between that source and the main source. If the difference gets higher than 3 Volt, main VDD is pull up, so the 4 Volt limit will not be reached.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.