2018-03-12 4:46 AM
Hello,
I want to write a 'User Application' for the USART bootloader (
AN4657
) provided by ST.I modifed the CubeMX generated code like below;
My code is not working properly. When I debug my code, I see that HAL_IncTick() is never called. I see that my code is waiting in HAL_Delay() because of not working systick count.
What could be the problem in my code ?
Main.c
------------------------------------------------------------------
#define APPLICATION_ADDRESS (uint32_t)0x08004000
__IO uint32_t VectorTable[24] __attribute__((at(0x20000000)));
for(i = 0; i < 24; i++)
{ VectorTable[i] = *(__IO uint32_t*)(APPLICATION_ADDRESS + (i<<2)); }stm32f042x6_flash.icf
------------------------------------------------------------------
define symbol __ICFEDIT_intvec_start__ = 0x08004000;
define symbol __ICFEDIT_region_ROM_start__ = 0x08004000;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.