STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem in file system update using UART in SPWF01S

Posted on March 12, 2018 at 15:11In SPWF01S wifi module, could perform File system update using AT+S.HTTPDFSUPDATE over the air with the help of Apache web server successfully (from Lab6 of Wi-Fi Training - Hands On  manual). But the same is giving ...

How to single stepping debug STM32F091

Posted on March 09, 2018 at 14:33 I have several STM32 CubeMX / HAL projects and I use EmBitz as IDE. All porjects working fine, including compilation and debugging. There are projects with STM32F103, STM32F205, STM32F207,STM32F405, STM32F429, STM3...

use dfsdm with parallel input

Posted on March 11, 2018 at 16:38Hi,I have get pdm data and want to use dfsdm to convert to PCM.The test code is like below:HAL_DFSDM_FilterRegularStart(&hdfsdm1_filter0); uint16_t *pdm_data=... for (int i=0;i<pdm_size;i++) { hdfsdm1_channel1.Instan...

hgyxbll by Associate II
  • 1784 Views
  • 2 replies
  • 0 kudos

issue with DCache on STM32F746ZG

Posted on March 11, 2018 at 16:54Hello, i'm having issue on STM32F746ZG, connected with ETH PHY through RGMII, and i'm having also enabled USB HS using ULPI, when i not enable DCache at start everything works perfectly ...but when i enable SCB_Enabl...

STM32F042 IAP Problem

Posted on March 12, 2018 at 12:46Hello,       I want to write a 'User Application' for the USART bootloader (AN4657) provided by ST.        I modifed the CubeMX generated code like below;       My code is not working properly. When I debug my code, ...

Unable to retrieve the data from external flash

Posted on March 12, 2018 at 12:46I am using STM32L100 to interface the External Flash through SPI but unable to retrieve the data from flash, using SPI_I2S_SendData library function to send data and SPI_I2S_ReceiveData library  function to retrieve ...

Fastest IRQ response on STM32F04?

Posted on March 10, 2018 at 06:36Hi all,I'm trying to respond to an IRQ in the fastest way possible on an STM32F04. Configuring a GPIO as EXTI works, but there's a ~200ns delay even at highest priority, presumably due to the overhead of the IRQ and ...

STM32f746vg internal oascillators?

Posted on March 09, 2018 at 11:36Hi!I am currently developing a wireless sensor node with the STM32f746vgt6 MCU. As I understand from reading the data sheet it is possible to run the MCU on its internal oscillators instead of adding external crystal...

Not able to out the LSI clock

Posted on March 12, 2018 at 10:08 Hi, I was trying to out the clocks through MCO pin of STM32F0. Got HSE, HSI, SYSCLK and PLLDiv2. But i am not able to out the LSI clock. Can you help me? The code i had used is as follows. Hi, I was ...

INDHU N by Associate
  • 695 Views
  • 0 replies
  • 0 kudos

Nucleo32 Sleep

Posted on March 10, 2018 at 18:53Hello,I have the Nucleo L43KC MCU. Is there any way I can put it into sleep or standby or other power modes? I noticed it doesn't have a wakeup pin unfortunately after I bought itThanks

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.