2021-08-03 3:53 AM
Hello All,
We design a circuit with STM32F030F4.
And when I checked the current consumption of the circuit , I saw the curent consumption is changing by the time.It moves like decreasing for some time and increasing suddenly after that decreasing for some times again and increase again.And it repeats this continiously.MCU is using internal crystal.
I check all circuit and find the cause.It does that because of PLL.
Because I check this status:
1) With 8 MHz without PLL
and current consumption is standing still and its value is 0.6 mA
2) With 8 MHz with PLL
and current consumption is floating and its value is 0.8 mA
When we use PLL current consumption is increase and floating.
When the clock speed is set higher value than fluctuation in the current is also increase.
Is there any information about this .
Can we stop this fluctuation .
Any advice would be helpfull,
Thank you.
Regards.
EMRE
Solved! Go to Solution.
2021-08-03 6:00 AM
Dear EMRE,
This fluctuation in Run/dynamic mode is normal behavior and the consequence of a regulation loop of our internal LDO of few seconds. to be completely sure You need to run in sleep mode as example while Cortex-M0 is stopped and no variation due to code execution from Flash and memories. The most important is to keep an average consumption inline with our datasheet : Typical and Max values ( Frequency and temperature). Hope it helps you.
Ciao
STOne-32
2021-08-03 6:00 AM
Dear EMRE,
This fluctuation in Run/dynamic mode is normal behavior and the consequence of a regulation loop of our internal LDO of few seconds. to be completely sure You need to run in sleep mode as example while Cortex-M0 is stopped and no variation due to code execution from Flash and memories. The most important is to keep an average consumption inline with our datasheet : Typical and Max values ( Frequency and temperature). Hope it helps you.
Ciao
STOne-32
2021-08-03 11:39 PM
Hi Ciao,
Thanks for information.
I accept this fluction is normal than.
I learned a new information with this.
Have a nice day.
By By.
EMRE
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.