2025-01-31 11:11 PM
Greetings
I am using STM32F030C8T6TR for ADC on two channels IN1 & IN3. It works. However I wanted to add DMA.
When trying to add DMA , It shows on two channels channel 1 and channel 2 , Though the datasheet mentions DMA is available for 5 channels. I can add DMA for channel 1 - Peripheral to memory. However when I try to add a DMA for another channel It shows error "No DMA available for this peripheral".
I could add DMA for the above channels in Memory to memory mode.for the ADC though. Is this OK can It my understanding that when using ADC, peripheral to memory should be used. In which case I can add only one of the two channels - channel 1 or channel 2.
How does this work ? will memory to memory on both channels work as expected ?
or is this some kind of version related error ? I use STM32CubeIDE1.15.0 on windows 7.
Thank you.
2025-02-03 7:58 AM
Sorry for the typing Mistake : NOT STMLink. It is ST-Link V2. Oh! it is available at just about $2 /-. I think it is some chineese clone, because the controller is not from STM. However it works.
2025-02-10 7:12 AM
Hello guys,
Got it working . Both Polling Method and DMA too.
Strangely , I could debug too using the obsolute cheap ST-Link V2 with openCD. It never used to work. It took some pretty good effort to make it work. .
Thanks a lot for all your participation.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.