cancel
Showing results for 
Search instead for 
Did you mean: 

Change OSC_IN pin with OSC32_IN ?

hazall
Associate III

I am using STM32F030C8T6TR. An external 8 mhz oscillator was connected to the OSC_32_IN-OUT input by mistake, not to the OSC_IN-OUT pins on the board I have. Hardware cannot be changed. Can I reconfigure the pin with software or How can I use it? I am new in stm32.

Thanks from now :)

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

The oscillator pins are fixed and not interchangeable. Only the GPIO alternative can be selected. In this respect, you will have to make a new layout.

Hope that helps?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.