2022-03-15 2:05 AM
I would like to put STM32F030K6T6 into STOP mode (low power mode), in which there should be current consumption around 5 μA.
But whatever I do the current consumption is around 450 μA in stop mode.
There is basically nothing else on the PCB, it's as simple as possible.
The board without MCU consumes 7 μA, that is quiescent current of LDO. So in the end I would expect to get 12 μA (7 + 5 μA).
When I place there MCU the consumption is around 2-3 mA in normal mode and 450 μA in stop mode.
All pins are set to analog input with no pull-ups, which is recommended config. All peripherals are disabled (like ADC, IWDG, I2C, SPI, timer, etc.). Only RTC is enabled.
I tried it with all pins set to output, it did not help either.
What do I do wrong?
int main(void) {
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_RTC_Init();
while (1) {
goto_stop();
HAL_Delay(3000); // 3 seconds of full power
}
}
void goto_stop(void) {
RTC_DateTypeDef sDate;
sDate.Date=1;
sDate.Month=RTC_MONTH_JANUARY;
sDate.Year=22;
sDate.WeekDay=RTC_WEEKDAY_MONDAY;
// HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD);
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BIN) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
RTC_TimeTypeDef sTime;
sTime.Seconds=0;
sTime.Minutes=0;
sTime.Hours=0;
// HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD);
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BIN) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
HAL_NVIC_EnableIRQ(RTC_IRQn);
RTC_AlarmTypeDef sAlarm;
sAlarm.Alarm=RTC_ALARM_A;
sAlarm.AlarmTime.Seconds=20;
sAlarm.AlarmTime.Minutes=0;
sAlarm.AlarmTime.Hours=0;
// sAlarm.AlarmMask=RTC_ALARMMASK_SECONDS | RTC_ALARMMASK_MINUTES | RTC_ALARMMASK_HOURS;
sAlarm.AlarmMask=RTC_ALARMMASK_HOURS | RTC_ALARMMASK_DATEWEEKDAY;
// HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD);
sAlarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET;
sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL;
sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE;
if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BIN) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
__HAL_RCC_GPIOA_CLK_DISABLE();
__HAL_RCC_GPIOB_CLK_DISABLE();
__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOD_CLK_DISABLE();
__HAL_RCC_GPIOF_CLK_DISABLE();
HAL_SuspendTick();
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
SystemClock_Config();
HAL_ResumeTick();
}
Solved! Go to Solution.
2022-03-20 10:43 AM
That means both answers (mine and your) are correct. When that setting is enabled, at connection the debugger sets the respective bits in DBGMCU_CR register.
Still take a note that DBGMCU_CR register is not reset by system reset. That means it will be reset only by removing the power and waiting for the capacitors to discharge. Depending on the schematics and power consumption, for some devices it can take many seconds or even minutes.
2022-03-20 10:48 AM
I tried
DBGMCU->CR=0;before, it did not help.
Well, actually I was not able to flash with this line in the code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.