2018-05-05 7:50 AM
Hi All.
I am using STM32F030 as my development platform. I have a RF module connected to UART2.
The uart is operating at 9600, UART_RX is configured as interrupt. Things work fine, but sometimes a global buffer defined as static in some other file is getting corrupted with values received over UART.
Any inputs on finding the issue will be of great help?
Thanks.!
#stm32 #stm32-uart #memory-corruption2018-05-05 8:23 AM
Watch the pointer used in the receiving UART function. Seems like it exceeded boundaries of the memory where you would like to store data received from the UART.
Share the code to understand the role of the buffer vs place in the memory you want to store UART received data.
2018-05-05 11:50 AM
You're going to need to walk your code an identify memory usage and writes which could corrupt memory or go out of bounds.
You'd want to add checks and breakpoints in critical areas to sanity check pointers and indexes to ensure they don't go out of range, and secondary checks of the buffer getting corrupted to trap the failure as quickly as possible after it happens so you can zoom down and focus on specific portions of your code.
Make sure your stack is sufficiently large to manage your usual call tree, and any the would occur from interrupts. Quantify how much stack you are currently using.
Check memory as you enter and leave interrupts.
2018-05-07 2:03 AM
HI.
Thanks guys..!!!
Apparently i was getting UART overrun error and data getting missed. Due to this the uart rx buffer overflowing.
There was no overflow checks, my bad..!!!
I am still debugging...will update if i find anything.
Thanks..!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.