2015-10-28 6:57 AM
Hello everybody, with this code, no matter what I do, I always get 4095 (max). I've tried looking at Clive examples or IAR's examples I just can't see it. Could someone take a look and see what am I missing. I need to measure the internal reference voltage and one external channel seemed simple enough.
<code>/* ADC measurement */&sharpinclude ''stm32f0xx.h''&sharpdefine SAMPLES 2&sharpdefine RECEIVE 1&sharpdefine TRANSMIT 0void GPIO_init();void ADC1_init();void init_DMA();void delay(uint32_t time);uint16_t ADC1ConvertedValue[SAMPLES] = {0};uint16_t ADC1Average = 0;uint8_t ADCCounter = 0;uint8_t* ADCDataOut;uint32_t VREFINT_CAL;uint32_t tempADC;uint16_t Vrefint_voltage;uint32_t ADCVref_kvant;int main(){ GPIO_init(); init_DMA(); ADC1_init(); VREFINT_CAL = (*(uint16_t*)0x1FFFF7BA); Vrefint_voltage = 1542*3300/4095; while(1){ while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET); /* Get ADC1 converted data */ ADC1ConvertedValue[0] = ADC_GetConversionValue(ADC1); } }void GPIO_init(){ GPIO_InitTypeDef GPIO_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configure USART1 pins: Rx and Tx ----------------------------*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_1); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure);}void ADC1_init(){ ADC_InitTypeDef ADC_InitStruct; ADC_DeInit(ADC1); RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); ADC_StructInit(&ADC_InitStruct); ADC_InitStruct.ADC_Resolution = ADC_Resolution_12b; ADC_InitStruct.ADC_ContinuousConvMode = ENABLE; ADC_InitStruct.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStruct.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStruct.ADC_ScanDirection = ADC_ScanDirection_Upward; ADC_Init(ADC1, &ADC_InitStruct); ADC_ChannelConfig(ADC1, ADC_Channel_5, ADC_SampleTime_239_5Cycles); ADC_ChannelConfig(ADC1, ADC_Channel_Vrefint, ADC_SampleTime_239_5Cycles); ADC_VrefintCmd(ENABLE); ADC_GetCalibrationFactor(ADC1); /* ADC DMA request in circular mode */ ADC_DMARequestModeConfig(ADC1, ADC_DMAMode_Circular); /* Enable ADC_DMA */ //ADC_DMACmd(ADC1, ENABLE); ADC_Cmd(ADC1, ENABLE); while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_ADEN)); ADC_StartOfConversion(ADC1); }void init_DMA(){ NVIC_InitTypeDef NVIC_InitStruct; NVIC_InitStruct.NVIC_IRQChannel = DMA1_Channel1_IRQn; NVIC_InitStruct.NVIC_IRQChannelPriority = 0; NVIC_InitStruct.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStruct); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); DMA_InitTypeDef DMA_InitStructure; DMA_DeInit(DMA1_Channel1); DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_InitStructure.DMA_BufferSize = SAMPLES; DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&ADC1ConvertedValue[0]; DMA_Init(DMA1_Channel1, &DMA_InitStructure); DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE); DMA_Cmd(DMA1_Channel1, ENABLE); //Enable the DMA1 - Channel1}void DMA1_Channel1_IRQHandler(void){ if(DMA_GetITStatus(DMA1_IT_TC1)){ DMA_ClearITPendingBit(DMA1_IT_TC1); }}void delay(uint32_t time){ for(; time > 0; time--);}</code> #stm32f3-adc-vrefint-temp_sensor2015-10-28 10:32 AM
Okay, the external channel seems to show some hope (added some delays between measurements in the DMA interrupt), but the Vrefint still 4095.
2015-10-29 3:40 PM
Here i made this example for you. Tested and working on stm32f051R8 mcu. Hope this helps.
2015-10-30 2:29 AM
Hey, I found the problem last night, apparently on one of the pins, that was ''TTa'', which means only accepts 3.3V, there was a 5V drop. After I removed it the ADC started working just fine. Probably the voltage leaked into the ADC which then malfunctioned.
2016-05-01 4:07 AM
Hi,
I'm also facing this issue with board STM32F3 Discovery. Values from VREFINT and Temp Sensor are always 4095. I dont know why. Anyone who knows this issue, please help me. Thank you very much.2016-05-01 8:51 AM
When your question deviates significantly off-topic, into a different part, and many months ago, you should open a new thread.
Have you actually enabled the Vref/Temp sources? Show complete and concise code example demonstrating your problem.You want to find people who don't and haven't had this problem.2016-05-01 10:45 AM
2016-05-01 11:29 AM
Hi,
I've just posted my thread, but I don't see my thread appearing in the forum.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.