2016-03-18 12:17 AM
STM32F030x8, HAL v.1.5.0, UART Receiving by polling
If I take byte from RDR reg and reset RXNE rarely UART gets next byte, UART breaks down, and RXNE doesn't SET never (I do it by func HAL_UART_Receive(&RS485Handle, &byte, 1, 1000))I fix it by clearing ORE flag if tjis flag is SET in func UART_WaitOnFlagUntilTimeout in func HAL_UART_Receive.Why isn't it fixed still in HAL? UAR breaks down when overrun without this fix.2 ST programmers: can You include this fix to next HAL?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.