2015-01-18 10:42 PM
Hello everyone!
Help me, please. I've got STM32F042K6T6. Can I use it in anendpoint
device? Here is only CAN interface, is it possible to use it as slave? Thanks! #slave #bxcan #stm32f0 #slave #bus #can #can2015-01-19 5:07 AM
CAN is a peer to peer network, not sure what you mean by ''slave mode''. Some CAN software protocols do use a bus master to control startup and configure other nodes, but there is no hardware mode for a bus master other than having the highest priority.
Endpoints are in USB, not CAN. All CAN nodes support the same 11 bit or 29 bit object address space. Anything equivalent to an endpoint is entirely software dependent for the protocol used. Jack Peacock2015-01-19 10:59 PM
I had some
doubts
because of the
settings
of the
CAN-BUS in STM Cube. There only master mode could be selected.
Thanks for your answer! ________________ Attachments : CAN_STM_Cube.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0ua&d=%2Fa%2F0X0000000bfT%2F2AcOiTazzjRgy_roghtQHZhEjvGP.KoR.4pwL7yjAxU&asPdf=false2015-01-20 6:22 AM
Hello Sergey,
have you by any chance tried to initialize USB for VCP communication with STM32F042K6T6? I am quite stuck on it.2016-01-18 1:04 AM
Hi Sergey and others!
I have the same problem with STM32L476RG. To Select CAN I must Select Master, but I want a slave! Did you find a solution? Regards, Gerhard PS. ScreenShot attached ________________ Attachments : CubeMX_Selecting_Slave_CAN.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0uL&d=%2Fa%2F0X0000000bfR%2FgVGO4RUtN7E6pEj0TnOd3RNFvqpGcN_wMSoLo0IJx1E&asPdf=false2016-01-18 5:54 AM
But what does ''Slave'' even mean in your context? The CAN device can listen to device traffic in it's standard configuration. Whether you send messages onto the bus is entirely up to you, so just listen and don't send anything.
2016-01-21 4:02 AM
I thought slave was an ordinary term in CAN, even though they use several concepts: Master / Slave, Client / Server, Producer / Consumer.
The slave will typically be a sensor. The Master requests data from the sensor. However, I didn’t expect the master / slave to have any influence at this low level. At this level I expected an driver and receiver and no difference between master and slave. Regards, Gerhard P.S. Sorry for the late answer. I am used to e-mail warnings when I get reply in forums. I realized I needed to select it here.2016-01-21 4:34 AM
The basic CAN does not have master/slave devices, just address based arbitration. OTOH, higher level protocols like CANopen --do-- have a master/slave concept.
I never used the STM32 CAN peripheral, so I'm not sure if ST mixed in such a concept. I recommend to read the reference manual here.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.