2017-02-07 10:33 AM
I have a Nucleo STM32F303RE that I'm using with the Eclipse IDE. I've downloaded and installed the STM32CubeMX plug-in, but I have idea how to activate it to take advantage of it....
Are there any step-by-step examples that show how to make use of CubeMX in Eclipse?
Is the CubeMX plug-in compatible with the GNU ARM Eclipse tools?
Thanks!
-Eric
2017-02-07 11:03 AM
For a quickstart, you could just use TrueStudio instead. That's basically an eclipse IDE with all required plugins bundled up for embedded development. I'm using it and it's great so far. Only once you want to do some advanced debugging, e.g. with RTOS, there are some limitations in the free version. But it gets you pretty far and if those limitations become important, one could still change back to a self-bundled eclipse install.
At least it gets you started.
Just select truestudio project as output in CubeMX and then import that project into your workspace.
2017-02-07 9:26 PM
Well, thanks, that's one option. But what's the process if I want to use Eclipse?
Do I need to use CubeMX outside of Eclipse and then import the files? (But then, what's the point of the plug-in?)
How do I take advantage of the plug-in feature?
Thanks!
2017-02-08 1:02 AM
Hello,
to install the plugin in eclipse,
Now to see CubeMx application inside eclipse as a persperctive you may have to go to the menu:
Window/ > Perspective > Open Perspective > Other... and then choose STM32CubeMx
This should work on any IDE base on eclipse (like True Studio, SW4STM32, ...)
Best regards,
Max
2017-02-08 5:55 AM
Excellent, thanks!
Opening it as a Perspective was what I was missing. I don't think I've seen any documentation anywhere suggesting that's where it would show up, and I can't think of how frustrated I would have to be before I randomly looked there.
I see that there are a dozen or so other Perspectives.... I've used the Code and Debug ones, but I guess I still have a lot to learn about using Eclipse!
-Eric
2017-02-08 8:49 AM
Use System Workbench a free ide and gcc compiler. Simply start new project with CubeMX select SW4STM32 as toolchain and open your project. Get SW at openstm32.org
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.