2016-02-06 7:30 PM
Yesterday I upgraded to V4.13.0 which required that I also upgrade to STM32CubeL4 V1.3.0.
Since then, every project that I generate exhibits a couple of problems:1) every reference to RCC_xxx #defines shows up in the IDE as ''Type RCC_xxx could not be resolved''. Same with anything that looks like it could be a system defined preprocessor symbol. The programs compile OK so I think this is an issue with the generated code for the project2) every program starts in debug and, before it gets to the 'main' function, ends up in the ''startup_stm32L476xx.s'' file at some labels called ''Default_Hander:'' and ''Infinite_Loop:'' where the executable code is exactly that - a branch back to the label. I have single stepped through the code form the ''Reset_Handler:'' label and the last statement seems to cause the problem is ''bi __libc_init_array'' in that I cannot step into that function and when I pause the processor I'm at the infinite loop.The console shows:===================================Breakpoint 1, LoopFillZerobss () at C:/Users/Administrator/workspace/Blinky/Drivers/CMSIS/Device/ST/STM32L4xx/Source/Templates/gcc\startup_stm32l476xx.s:114
114 bl __libc_init_array
Program received signal SIGINT, Interrupt.
WWDG_IRQHandler () at C:/Users/Administrator/workspace/Blinky/Drivers/CMSIS/Device/ST/STM32L4xx/Source/Templates/gcc\startup_stm32l476xx.s:134
134 b Infinite_Loop
===========================Have I done something or not done something that has caused this?Susan2016-02-22 6:01 PM
Thanks - I'd like to try that. However, are you referring to the 'LinkerScript.ld' file or 'STM32L476VGTx_FLASH.ld' file. Looking at your code, I can't see that it is a modification to either file (yours looks totally different to either of those files and I don;t have the knowledge to determine if they really are the same) and a search of all of the generated files does not show the
''__stack'' or ''_estack'' symbols
.(Edit: oops - actually I can see the '_estack' but not the '__stack' symbol)However, and with all due respect, I do not think a work-around is the correct way to go.If this is a 'bug' then it needs to be acknowledged and fixed.If it is NOT a bug, then I really would appreciate knowing what I am doing wrong to get into this situation.Susan2016-02-22 9:20 PM
replace content of STM32L476VGTx_FLASH.ld with this file and it works. _estack in cubemx linker is totally wrong and will get you into infinite loop. If you prefer to modify linker generated by CubeMX change RAM size to 96K and _estack to 0x20017FFF
2016-02-23 2:27 AM
Dear Susan,
The L476VGTx MCU has 2 RAMs and indeed the linker script is wrong and you should follow the recommendation: RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 96K CCMRAM (xrw) : ORIGIN = 0x10000000, LENGTH = 32K This will be fixed in STM32CubeMX 4.14. Thank you for the details you provided.2016-03-22 11:08 AM
Please note STM32CubeMX 4.14 implements a workaround to the linker script issue on RAM descriptions: only RAM1 will be listed with 96k size. In a next release, both RAMs will be made available in the linker script.
Best regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.