2016-03-02 10:28 PM
Hello.
CubeMX not correct settings SDRAM, when use 2 chip.CubeMX create next not work code:/* FMC initialization function */
void MX_FMC_Init(void){ FMC_SDRAM_TimingTypeDef SdramTiming; /** Perform the SDRAM1 memory initialization sequence */ hsdram1.Instance = FMC_SDRAM_DEVICE; /* hsdram1.Init */ hsdram1.Init.SDBank = FMC_SDRAM_BANK1; hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_9; hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_13; hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_16; hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4; hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3; hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE; hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2; hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE; hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_1; /* SdramTiming */ SdramTiming.LoadToActiveDelay = 2; SdramTiming.ExitSelfRefreshDelay = 7; SdramTiming.SelfRefreshTime = 4; SdramTiming.RowCycleDelay = 7; SdramTiming.WriteRecoveryTime = 3; SdramTiming.RPDelay = 2; SdramTiming.RCDDelay = 2; HAL_SDRAM_Init(&hsdram1, &SdramTiming); /** Perform the SDRAM2 memory initialization sequence */ hsdram2.Instance = FMC_SDRAM_DEVICE; /* hsdram2.Init */ hsdram2.Init.SDBank = FMC_SDRAM_BANK2; hsdram2.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_9; hsdram2.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_13; hsdram2.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_16; hsdram2.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4; hsdram2.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3; hsdram2.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE; hsdram2.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2; hsdram2.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE; hsdram2.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_1; /* SdramTiming */ SdramTiming.LoadToActiveDelay = 2; SdramTiming.ExitSelfRefreshDelay = 7; SdramTiming.SelfRefreshTime = 4; SdramTiming.RowCycleDelay = 7; SdramTiming.WriteRecoveryTime = 3; SdramTiming.RPDelay = 2; SdramTiming.RCDDelay = 2; HAL_SDRAM_Init(&hsdram2, &SdramTiming);}Need befor Init sdram2, then init sdram1.
Next cod is work:/* FMC initialization function */void MX_FMC_Init(void){ FMC_SDRAM_TimingTypeDef SdramTiming; /** Perform the SDRAM2 memory initialization sequence */ hsdram2.Instance = FMC_SDRAM_DEVICE; /* hsdram2.Init */ hsdram2.Init.SDBank = FMC_SDRAM_BANK2; hsdram2.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_9; hsdram2.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_13; hsdram2.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_16; hsdram2.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4; hsdram2.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3; hsdram2.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE; hsdram2.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2; hsdram2.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE; hsdram2.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_1; /* SdramTiming */ SdramTiming.LoadToActiveDelay = 2; SdramTiming.ExitSelfRefreshDelay = 7; SdramTiming.SelfRefreshTime = 4; SdramTiming.RowCycleDelay = 7; SdramTiming.WriteRecoveryTime = 3; SdramTiming.RPDelay = 2; SdramTiming.RCDDelay = 2; HAL_SDRAM_Init(&hsdram2, &SdramTiming); /** Perform the SDRAM1 memory initialization sequence */ hsdram1.Instance = FMC_SDRAM_DEVICE; /* hsdram1.Init */ hsdram1.Init.SDBank = FMC_SDRAM_BANK1; hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_9; hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_13; hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_16; hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4; hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3; hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE; hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2; hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE; hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_1; /* SdramTiming */ SdramTiming.LoadToActiveDelay = 2; SdramTiming.ExitSelfRefreshDelay = 7; SdramTiming.SelfRefreshTime = 4; SdramTiming.RowCycleDelay = 7; SdramTiming.WriteRecoveryTime = 3; SdramTiming.RPDelay = 2; SdramTiming.RCDDelay = 2; HAL_SDRAM_Init(&hsdram1, &SdramTiming);}I hope you resolve the problem and make a little better cubeMX.2016-03-08 1:14 AM
Hi drachev.andrei,
Your case is reported internally for further investigation.You will be updated if there are more details to add on this regard.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-03-18 1:21 AM
Dear user,
Thank you for reporting this issue. Your workaround is correct. The root cause has been found in the HAL driver implementation and shall be fixed a.s.a.p.: The SDRAM2 configuration is clearing the whole configuration of bank1 when it should only take care of the parameters for both banks(clock period, burst...): these parameters are configured in SDCR1 register. Best regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.