2018-05-03 9:02 AM
Hi,
I am using STM32CubeMX generated code run on Nucleo-144 board for STM32L496ZGT MCU. When I just have 3 UART enabled in cube, the code seems work fine. After I have added more components to the cube, the code go to an startup_stm32l4a6xx.s code. Seems a exception.
Here is the init code. The issue starting MX_LPUART1_UART_Init(). If I comment this out, will exception other init code too.
Any thoughts on this failure?
Thanks,
****
/* Initialize all configured peripherals */
MX_GPIO_Init(); MX_ADC1_Init(); MX_ADC3_Init(); MX_AES_Init(); MX_CRC_Init(); MX_HASH_Init(); MX_I2C1_Init(); MX_I2C2_Init(); MX_IWDG_Init();MX_LPUART1_UART_Init(); MX_UART4_Init(); MX_UART5_Init(); MX_USART1_UART_Init(); MX_USART2_UART_Init(); MX_USART3_UART_Init(); MX_QUADSPI_Init(); MX_RNG_Init(); MX_RTC_Init(); MX_SPI1_Init(); MX_SPI2_Init(); MX_WWDG_Init();/* Zero fill the bss segment. */
FillZerobss: movs r3, #0 str r3, [r2], #4LoopFillZerobss:
ldr r3, = _ebss cmp r2, r3 bcc FillZerobss Note: this post was migrated and contained many threaded conversations, some content may be missing.Solved! Go to Solution.
2018-05-24 11:33 AM
I figured out it's the compiler optimization issue. After turn it off, then it works as expected. Thx
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.