2014-06-11 3:56 AM
2014-06-11 11:33 PM
This bug isn't only for software STM32CubeMX 4.2.0 but for library STM32Cube F4 v1.1.0
HAL_xxx_CLEAR_IT( ) macro is incorrectTIMER, ADC, I2C, SPI, TIM, UART, USART, WWDG=====https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSTM32Java%2fSTM32F4xx%20HAL_TIM_IRQHandler%20misses%20interrupts%20on%20nearly%20overlapping%20TIM%20interrupts&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E...2014-06-14 10:41 AM
I found another bug:
When configuring SPI (at least SPI3, I didn't test the others) the generated code fails because hspi3.Init.CRCPolynomial is not set, which leads to a failed assertion in HAL_SPI_Init.edit:Also, when MCO2 is configured with PLLI2SCLK as source, no code for the PLLI2S configuration is created, if no I2S instance is configured.2014-06-17 9:03 AM
Initialization of ADC1 for SRM32F401RE fails because multimode.DMAAccessMode is not set in in main.c function MX_ADC1_Init().
This causes assert_param() to fail in HAL_ADCEx_MultiModeConfigChannel().We’re moving the ST Community to a new platform to give you a better and more reliable community experience.