STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN driver

Posted on June 18, 2014 at 11:57So if I want to connect two discovery boards, Could I use this sample? I have to use 2 CAN driver?!!

0690X00000605YvQAI.png
hamed by Associate II
  • 650 Views
  • 0 replies
  • 0 kudos

SPI interruption problem

Posted on April 04, 2014 at 16:43Hi all,I would like to know if anyone has a problem when enabling the Tx buffer empty interrupt. In fact, when i put SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_TXE, ENABLE);  , the code coming after can't be executed switch (...

ULPI HS-USB and I2S

Posted on June 17, 2014 at 05:07Without delving into the DS, can someone please confirm for me whether you can or cannot have ULPI and I2S enabled at the same time with F2-F4 QFP144 and smaller?This seems a bit odd since I think there would be a nee...

STM32F205 Power Stop example does not work

Posted on June 17, 2014 at 17:47Hello, I am currently trying to get the example code for Stop mode for the STM32F2xx processor to work, without success. The example in question is the Stop.ewp project. The Wakeup IRQ handler is never called and the ...

gerald2 by Associate
  • 1189 Views
  • 2 replies
  • 0 kudos

Looking for alternative STM32 peripheral libraries

Posted on June 12, 2014 at 16:11Hi, I'm in a project were we would like to use the STM32F103TBU7. As a toolchain we would like to use the IAR Embedded Workbench. Sadly I'm not allowed to use the STM peripheral library. This because it's a security a...

STM32CubeMX 4.2.0 Known Issues

Posted on June 11, 2014 at 12:56The original post was too long to process during our migration. Please click on the attachment to read the original post.

joe by Associate III
  • 2308 Views
  • 3 replies
  • 0 kudos

SPI with DMA

Posted on June 13, 2014 at 16:30Hello; I want to use DMA to transmit and receive data between a Slave and Master STM32 Boards. My question is how can i configure the DMA to transfer many different Array for example? i mean i want the slave to send ...

HS-USB in STM3240G-EVAL

Posted on June 11, 2014 at 22:36Hi, I just got the STM3240G evaluation board and wanted to use it as a CDC USB device, for HS USB. I haven't had much success with ST's firmware so far. I generated the configuration files using the Cube application, ...

c_uimran by Associate II
  • 1861 Views
  • 3 replies
  • 0 kudos

lost gpio.c file after regenerate code

Posted on May 28, 2014 at 12:23Many times, but not always, when I modified some pin configuration in CubeMx and regenerate the code, I lost the gpio.c file. Anybody can help?

matianfu by Associate II
  • 2009 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.