2016-04-25 11:50 PM
Hi,
As per UM1749 User Manual (Description of STM32L0 HAL and Low-layer drivers) the Low Level API should be found in: ''The Low Layer files are located in the same HAL drivers folder'' Figure 8: Low Layer driver folders'' Unfortunately there is no STM32l0xx_ll_.... files in this package. Where can I find them? Thanks, BogdanSolved! Go to Solution.
2016-05-25 3:10 AM
Hi golab.bogdan,
Thr LL drivers are available now with STM32CubeL0 V1.6.0 -Hannibal-2016-04-26 10:41 PM
I verified that LL drivers are available in Cubex package for STML4. So it seems that in L0 package these LL drivers are missed (the supposed to be there in the L0 HAL & LL user guide).
Not sure where to report this issue.2016-05-02 1:51 AM
Hi golab.bogdan,
The Low Layer driver is not yet generated, that will be published on the web by end of the month. The document is update a little bit early. Sorry for the inconvenience. -Hannibal-2016-05-25 3:10 AM
Hi golab.bogdan,
Thr LL drivers are available now with STM32CubeL0 V1.6.0 -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.