STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 USB device not being detected

Posted on May 25, 2016 at 13:23Hi All,I'm using a STM32F7 Discovery board. I am using the example application (unmodified) from Cube for being a USB MSC device.When I run the code with the debugger connected (using ST Link) everything works as expec...

STM32F411RC SRAM or FLASH USE to store static data

Posted on May 24, 2016 at 12:55Hello Everyone, I am using STM32F411RC. Here i want to store a variable as static. We can say that if we power off the MCU then also it will have same variable. how can i do that. I want to Read and write in SRAM or Fl...

jay1991 by Associate II
  • 3850 Views
  • 9 replies
  • 0 kudos

STM32F429BIT6 HSE Oscillator problem

Posted on May 24, 2016 at 12:23Hi I am having problems getting the external crystal oscillator to run correctly. It has a dc offset of approx. 1.5V but a peak to peak of only 380mV. The circuit is based on the STM32F429 Discovery board which produce...

HAL_SPI_Transmit

Posted on May 18, 2016 at 22:44Hello, We want to use HAL_SPI_Transmit function to load the data from 16 bit Array.  The function parameters are (SPI_Handle TypeDef *hspi, uint8_t * pdata, uint16_t Size, uint32_t Timeout). Our data buffer is defined ...

vimmi by Associate II
  • 2386 Views
  • 3 replies
  • 0 kudos

LTDC-TFT CONTROLLER

Posted on May 24, 2016 at 17:57Hi,I'm using a stm32f429ZIT discovery with the tft.I'm trying to configure the tft. I have a conflict between the usart2_CTS and LTCD_G7.I don't have any usart free, then I need to change the LTCD_G7 to another pin. Th...

cricart by Associate II
  • 1067 Views
  • 1 replies
  • 0 kudos

Reconfigure the timer at runtime

Posted on May 24, 2016 at 16:03I'm use STM32CubeMX to configure TIM2 CH1 to compare output, and it works well. Now I want to change it to PWM output when the programm running. Then which HAL library function to call to clear the registers previous s...

CUBEMX ADC

Posted on May 23, 2016 at 23:14Hi, I have started to work with STM32L1. Maybe it's a silly questestion, but how to read multiple ADC channels without DMA? It is simple to read 1 channel with HAL_ADC_GetValue(&hadc); or multiple channels with DMA HAL...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.