2015-04-28 11:37 AM
We are using the same SDRAM on our board as stm32f429i-disco and my question is about
the example code - STM32F429I-Discovery/Examples/FMC/FMC_SDRAM/Src/main.c where the initialization is only for BANK2, please confirm. Has anybody used and can provide the initialization for all 4 banks of IS42S16400J SDRAM ? stm32f4xx_ll_fmc.h only provides for BANK1 and BANK2: /** @defgroup FMC_SDRAM_Command_Target FMC SDRAM Command Target * @{ */ &sharpdefine FMC_SDRAM_CMD_TARGET_BANK2 FMC_SDCMR_CTB2 &sharpdefine FMC_SDRAM_CMD_TARGET_BANK1 FMC_SDCMR_CTB1 &sharpdefine FMC_SDRAM_CMD_TARGET_BANK1_2 ((uint32_t)0x00000018) /** * @} */ main.c calls the initialization : static void SDRAM_Initialization_Sequence(SDRAM_HandleTypeDef *hsdram, FMC_SDRAM_CommandTypeDef *Command) { __IO uint32_t tmpmrd =0; /* Step 3: Configure a clock configuration enable command */ Command->CommandMode = FMC_SDRAM_CMD_CLK_ENABLE; Command->CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2; Command->AutoRefreshNumber = 1; Command->ModeRegisterDefinition = 0;
The 64-Mbit SDRAM is a high speed CMOS, dynamic random-access memory designed to operate in 3.3 V memory systems containing 67,108,864 bits. it is internally configured as a quad-bank DRAM with a synchronous interface. Each 16,777,216-bit bank is organized as 4,096 rows by 256 columns by 16 bits. The 64-Mbit SDRAM includes an AUTO REFRESH MODE, and a power-saving, power-down mode. All signals are registered on the positive edge of the clock signal, CLK.
The STM32F429ZIT6 MCU reads and writes data at 80 MHz.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.