2016-10-23 12:38 PM
2016-10-23 10:18 PM
Solved,
The problem was in SDIO Clock Division its default value is 0 and it is usually too fast for SDCard to work with. I tested with 6 instead of 0 and it worked. The size of stack memory also should be higher than its default value(0x200)... I tested with 0x800 and it workedWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.