STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32446RE Nucleo as a USB CDC device

Posted on October 24, 2016 at 16:41Hi Guys,i try to experiment a bit with the USB CDC library. Sadly I don't get it to work out of the box after I configured everything in STMCubeMX.I tried to learn something from the F4 firmware libraray tutorial p...

STM32F746G Discovery UART MIDI

Posted on October 24, 2016 at 01:00 Hi. I'd like to use the UART for MIDI input. I've configured the UART on my STM32F7-Discovery board and perform a led toggle whenever an incoming message is received. I'm using the interrupt mo...

set peripheral interrupt priority higher than systick?

Posted on October 24, 2016 at 09:29Can I ask an easy question,that I found the systick CMSIS interrupt number is  -1and in NVIC_SetPriority(), the negative interrupt number will operate different with positive interrupt number So, can I set peripher...

ctc.ctc by Associate II
  • 768 Views
  • 1 replies
  • 0 kudos

Sequential Read of ADXL345

Posted on October 23, 2016 at 23:44 Hello, I am having problems reading the 6 output registers sequentially using the HAL drivers. I am able to read them one at a time without problems, but can't seem to get the sequential thing working? I'm usi...

uClinux on Custom board based-on stm32f746NGH.

Posted on July 12, 2016 at 20:13 Hi I have a STM32F746-DISCO and I ported uClinux from emcraft to it, run OK. But. In STM32F7-DISCO have only 8MB accessible because only 16bit data used. I have custom this board and using 32bit d...

STM32Cube FATFS Problem in STM32F103

Posted on October 23, 2016 at 21:38The original post was too long to process during our migration. Please click on the attachment to read the original post.

abbas by Associate II
  • 1363 Views
  • 1 replies
  • 0 kudos

File System on STM32F4xx nucleo

Posted on October 24, 2016 at 03:52Hello.I want to use FileSystem on STM32F4xx nucleo.but, as I have some restriction, I want to use RAM/ROM area for that, if possible.Could you let me know if any idea about such usage and any example source ?Regard...

s-shige by Associate II
  • 1187 Views
  • 1 replies
  • 0 kudos

Gain adjustment on audio line when using STM32F103

Posted on October 21, 2016 at 18:27Hi,I am having ADC3 bring in input from the microphone and I want to just the gain (amplitude) by 2 and then send it out through one of the DAC channels. So far, I have ADC and DAC synced through TIM8 and TIM6 resp...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.