2016-07-07 2:47 PM
Hi
I need to use the CN11 and CN12 connectors to use the FMC Bank 1 interface with an external memory board. Looking at the manual and schematic, it doesn't look like there's a way to disable the chip select on the eval board's SDRAM (which shares all of those connections on CN11 and CN12), which I need to do to use those connectors without also interacting with the eval board's SDRAM.Do you have any recommendations? Is there another chip select line I can use with FMC Bank 1 that doesn't connect to the on-board SDRAM?I saw a note about SB8 in the manual, but that doesn't seem to disconnect the microcontroller from the SDRAM's chip select line.ThanksBen2019-03-02 11:20 PM
Hi Ben,
Did you find any workable solution? I have same problem.
Regards,
MD
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.