STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F411 SPI RXNE bit is automatically clear

I'm very first to embedded programming, i have written a application using SPI protocol to communicate with 2 STM32F411 broads. And I got trouble in slave code, when the data from the master are sent to slave, then slave RXNE bit is set and go to SPI...

0690X000006DulSQAS.png 0690X000006DulNQAS.png

Resolved! HAL_NVIC_SystemReset() gets stuck, same with IWDG.

Hi. When I call HAL_NVIC_SystemReset(); or NVIC_SystemReset(); the system just freezes up instead of restarting. I figured forget about it and moved on to try out the watchdog, well the same thing happens. Watchdog is enabled and working fine, then I...

STM32CubeMX SD CARD Code Bug

Posted on January 31, 2018 at 12:48Hello,A while I used stm32cubemx for generating a code for SD card connection to my stm32f4 with SDIO and FATFS middleware and it worked fine but after the recent cube update the similar code does not works for sd ...

How to use eval board under windows 10

Hello,I used a STM32F103C8 eval board under windows 7 and everything worked fine. But I have to change to window 10 and I tried now for several hours to get a functional connection by reading many discussion of about stm32 vitual com port, etc.Can yo...

stop NRST pin being driven by flash programming algorithms.

It looks like I made a fatal mistake by connecting the NRST pin to the PA0 pin on an STM32F778AIY. This is a part with no internal voltage regulator for the core so the PA0 pin acts like a power on reset. This hasn't caused problems with power cyclin...

MVore by Associate II
  • 672 Views
  • 0 replies
  • 0 kudos

I2C base clock 8 / 16 / 48 / 100MHz? What to use best?

In the STM32H7 RM (July 2018) chapter 46.4.9 ("I2C_TIMINGR .. examples") you give example settings for i2c_ker_ck frequencies of 8 / 16 / 48MHz (thank you, very helpful - just a bit awkward that you use there the term "fI2CCLK" for the frequency ... ...

flyer31 by Senior
  • 1285 Views
  • 1 replies
  • 0 kudos

UWB Pulse

Hi.I want to generate an UWB pulse with 1ns pulse width and period of 1us.then i want to detect it.can stm32 help me to generate this pulse or detect a 1ns pulse ?sorry for bad English!

SRahm by Associate
  • 646 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.