2021-07-28 3:00 AM
i have integrated STL XCUBE class-B 2.2.0 Packages with STM32L433 controller here i am facing Startup RAM test issue
The RAM-test procedure STL_FullRamMarchC(RAM_START, RAM_END, BCKGRND) != SUCCESS) of the IEC 60335 SelfTest library ends with a HardFault Handler. when i run in debug mode end of the function return 1 then after jumping to Hard fault handler, i have checked RAM start end address correct only, what could be issue please help me out on ?
#define RAM_START ((uint32_t *)0x20000000uL)
#define RAM_END ((uint32_t *)0x2000BFFFuL) // 48KB used=>49151-1=0x2000BFFFuL
i have checked the application note AN4435 they mentioned changes regarding 2.3.0 only, there is no much information Xcube Class-B 2.2.0
if any help it would be grateful
Best Regards,
Naresh
Solved! Go to Solution.
2021-07-28 7:54 AM
Hi @Ssiva.2 ,
You will find an explanation for the faced issue in the article: ClassB example hard fault.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-07-28 7:54 AM
Hi @Ssiva.2 ,
You will find an explanation for the faced issue in the article: ClassB example hard fault.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.