2012-01-06 2:59 PM
I found that when output compare registers are loaded with a value that is more than ARR, then on overflow the timer automatically sets compare match interrupt flags. Has anyone seen it?
#stm32-timer-inerrupt2012-01-06 3:47 PM
I found that when output compare registers are loaded with a value that is more than ARR, then on overflow the timer automatically sets compare match interrupt flags. Has anyone seen it?
Isn't it documented?''Bit 1 CC1IF: Capture/Compare 1 interrupt flagIf channel CC1 is configured as output:
This flag is set by hardware when the counter matches the compare value, with some exception in center-aligned mode (refer to the CMS bits in the TIMx_CR1 register description). It is cleared by software.
0: No match.
1: The content of the counter TIMx_CNT matches the content of the TIMx_CCR1 register.
When the contents of TIMx_CCR1 are greater than the contents of TIMx_ARR, the CC1IF bit goes high on the counter overflow (in upcounting and up/down-counting modes) or underflow (in downcounting mode)
If channel CC1 is configured as input:
This bit is set by hardware on a capture. It is cleared by software or by reading the TIMx_CCR1 register.
0: No input capture occurred
1: The counter value has been captured in TIMx_CCR1 register (An edge has been detected on IC1 which matches the selected polarity)''
2012-01-09 7:28 AM
Thanks! Looks like my copy of RM0008 Reference manual is Rev 6 and badly outdated. It doesn't contain the clause about the CCR1 greater than ARR.
2013-07-24 7:02 AM
2013-07-24 7:19 AM
This really could have been a new thread.
You should setup the NVIC *before* enabling interrupt sources. Your timer settings are not correct, and you really want the larger divisor in the Period, having a Period of 1 is problematic. TIM_TimeBaseStructure.TIM_Period = 71; // 72 - 1 For 1us - 1 MHz timer TIM_TimeBaseStructure.TIM_Prescaler = 0; // Div 1 (Off - None) You're not conceivably going to be able to interrupt at 1 us, You can't do much in 72 cycles. For 1ms TIM_TimeBaseStructure.TIM_Period = 1000 - 1; // 1000 ticks at 1 MHz TIM_TimeBaseStructure.TIM_Prescaler = 71; // 72 - 1 For 1us - 1 MHz timer Don't use if-then-else construct in the interrupt handler, you may not arrive there for a singular event. If you want to measure something, the Period should be large, ideally 65535 (65536-1) so you can timestamp events based on the clocked counter. What are you going to be able to tell if the latched value is 0 or 1?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.