2013-07-23 12:42 PM
Hi, I've got some difficulties with wake uC up from stop mode. Firstly I copied example from Std Periph Library for STM32F103: it uses alarm from RTC to wake up. I implemented it and everything was OK. But next - I try to make the same in FreeRTOS - I change clock source for tick interrupt to RTC - alarms from RTC generate tick interrupts. I want to get into stop mode in idle hook function and wake up when alarm from RTC happens, but it doesn't work. I didn't change configuration of NVIC and EXTI. I'm clueless why...
Thanks for attention and help2013-07-23 2:38 PM
2013-07-24 4:29 AM
Ok, thanks, I'll try.
But does stop mode affect the configuration and operation of the RTC? I think it doesn't, so this is only to ensure2013-07-24 9:22 AM
You are correct, RTC function is kept active.
Cheers, STOne-32.2013-07-24 9:28 AM
The RTC however does have a dependency on the VBAT supply, and only LSE is in the backup power domain (F1/F2/F4). LSI will not tick when the primary regulators turn off.
2013-07-24 10:01 AM
Dear Clive,
Here we are in STOP mode, Only digital clocks are stooped, but Power domains are kept powered by VDD and regulator is always active ( either in RUN or LP modes). It seems the standalone example is working fine ( bare-metal) , but only when FreeRTOS is added, there is an issue. So I'm not suspecting Hardware, neither the device... Ciao, STOne-32.2013-07-24 11:09 AM
Thanks for reply,
regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.