2014-06-11 1:54 PM
Hi,
I used CubeMX 4.2 to generate code skeleton for L053. I have no problem with simple programs (LED blinking, etc). But I cannot use systick. I understand that HAL_init() takes care of setuping the systick. Unfortunately HAL_GetTick() does not return updated values. It seems that the systick interrupt is not initialized/enabled. Could you please share working examples for L053? I have no such issues using Standard Pheripheral Library on STM32F10x MCUs. Thanks, BogdanSolved! Go to Solution.
2014-06-13 9:15 AM
My fault. I have omitted the ''VECT_TAB_SRAM'' in C/C++->Preprocessor Symbols.
What a shame!2014-06-12 1:39 AM
[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx]STM32 Software Tools and Firmware''. No need to create new thread for this same topic, but this is to apply for new ones, if any :)
-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-06-12 9:43 AM
I tested one of the nucleo-L053 examples which uses HAL_Delay().
When the code is loaded via debugger to flash all works fine (the delay is used s I concluded that systick works fine). When the code is ran out of SRAM (loaded via debugger) it does not work. The program stops on HAL_Delay() function (I added some LED blinks before calling the HAL_Delay) so I am sure that it waits for tick update. It seems that tick counter is not updated. Strange because STM32F100RB works fine (systick works when run out of SRAM). ==== When I manually try to change the VTOC register value in KEIL (it seems to be not updated even though Dbg_RAM.ini is configured) I get: Internal DLL Error Internal command error Could an ST expert run the nucleo-L053 'GPIO_IOToggle' example out of SRAM in Keil IDE? I mean setting IROM to 0x20000000/0x1000, 0xIRAM to 0x20001000/0x1000 and configuring Dbg_RAM.ini in the debug tab, etc.2014-06-12 11:05 AM
Today Keil released new 5.11 version of IDE. This version has updated ST-link drivers for STM32L0.
Unfortunatelly after the update the keil cannot connect to the board (USB errors appears). It seems that I ran into another issue. The latest ST-link utility has no problem with connecting with the board;)2014-06-12 11:14 PM
I wonder if someone managed to run the nucleo-L053 'GPIO_IOToggle' example out of SRAM in Keil IDE? The idea is to try to run the code using systick (or other feature using NVIC/interupts) out of RAM.
I suspect that VTOC is not reconfigured correctly (the NVIC location is not moved to SRAM). It seems that the latest ST-link utility is able to do this. So it's rather an issue related to Keil (the latest 5.11 cannot communicate with nucleo at all, the 5.10 can do this to debug a program in the flash but cannot change VTOS - I guess). Again , if the program does not use interrupts the Keil 5.10 is able to place the code in SRAM and run it. So the issue is very subtle.2014-06-13 9:15 AM
My fault. I have omitted the ''VECT_TAB_SRAM'' in C/C++->Preprocessor Symbols.
What a shame!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.