2020-01-16 5:40 AM
I'm trying to read GPS-Data on the F429ZI that is sent from a GPS Module (NMEA GGA & VTG) with 38400 Baud but I only receive weird symbols. I tried sending specific values from my PC but they also turn into nonsense on the receive-side.
"U" (85dec / 1010101) is the only symbol that is received correctly. But when I try to send it back to the PC, it also changes value.
Equal values sent produce the same wrong value on the uC but I cant see a relation between sent and received values.
Some Examples:
255dec -> 0
0 -> 0
177dec ->69dec
65dec -> 95dec
I read a lot about these problems that were solved with a change in clock frequencies but cant't make it work for me with any frequency combination.
Thanks for your help!
(I modified a STM UART-Example for my purpose.)
main.h
/* Define to prevent recursive inclusion -------------------------------------*/
#ifndef __MAIN_H__
#define __MAIN_H__
/* User can use this section to tailor USARTx/UARTx instance used and associated
resources */
/* Definition for USARTx clock resources */
#define USARTx USART3
#define USARTx_CLK_ENABLE() __HAL_RCC_USART3_CLK_ENABLE()
#define USARTx_RX_GPIO_CLK_ENABLE() __HAL_RCC_GPIOB_CLK_ENABLE()
#define USARTx_TX_GPIO_CLK_ENABLE() __HAL_RCC_GPIOB_CLK_ENABLE()
#define USARTx_FORCE_RESET() __HAL_RCC_USART3_FORCE_RESET()
#define USARTx_RELEASE_RESET() __HAL_RCC_USART3_RELEASE_RESET()
/* Definition for USARTx Pins */
#define USARTx_TX_PIN GPIO_PIN_10
#define USARTx_TX_GPIO_PORT GPIOB
#define USARTx_TX_AF GPIO_AF7_USART3
#define USARTx_RX_PIN GPIO_PIN_11
#define USARTx_RX_GPIO_PORT GPIOB
#define USARTx_RX_AF GPIO_AF7_USART3
#define USER_Btn_Pin GPIO_PIN_13
#define USER_Btn_GPIO_Port GPIOC
#define LD3_Pin GPIO_PIN_14
#define LD3_GPIO_Port GPIOB
#define LD2_Pin GPIO_PIN_7
#define LD2_GPIO_Port GPIOB
/* ########################## Assert Selection ############################## */
/**
* @brief Uncomment the line below to expanse the "assert_param" macro in the
* HAL drivers code
*/
/* #define USE_FULL_ASSERT 1U */
#ifdef __cplusplus
extern "C" {
#endif
void _Error_Handler(char *, int);
#define Error_Handler() _Error_Handler(__FILE__, __LINE__)
#ifdef __cplusplus
}
#endif
#endif /* __MAIN_H__ */main.c
UART_HandleTypeDef UartHandle;
char RxByte;
void SystemClock_Config(void);
void USART3_IRQHandler(void)
{
HAL_UART_IRQHandler(&UartHandle);
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef* huart)
{
if (huart->Instance == USART3)
{
/* Receive one byte in interrupt mode */
HAL_UART_Receive_IT(&UartHandle, &RxByte, 1);
HAL_UART_Transmit_IT(&UartHandle, &RxByte, 1);
}
}
int main(void)
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/*##-1- Configure the UART peripheral ######################################*/
/* Put the USART peripheral in the Asynchronous mode (UART Mode) */
/* UART configured as follows:
- Word Length = 8 Bits (7 data bit + 1 parity bit) :
BE CAREFUL : Program 7 data bits + 1 parity bit in PC HyperTerminal
- Stop Bit = One Stop bit
- Parity = ODD parity
- BaudRate = 9600 baud
- Hardware flow control disabled (RTS and CTS signals) */
UartHandle.Instance = USARTx;
UartHandle.Init.BaudRate = 38400;
UartHandle.Init.WordLength = UART_WORDLENGTH_9B;
UartHandle.Init.StopBits = UART_STOPBITS_1;
UartHandle.Init.Parity = UART_PARITY_NONE;
UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
UartHandle.Init.Mode = UART_MODE_TX_RX;
UartHandle.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&UartHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
HAL_UART_MspInit(&UartHandle);
/* Peripheral interrupt init*/
HAL_NVIC_SetPriority(USART3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USART3_IRQn);
if (HAL_UART_Receive_IT(&UartHandle, &RxByte, 1) != HAL_OK)
{
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, 1);
}
/* Infinite loop */
while (1)
{
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
/**Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 16;
RCC_OscInitStruct.PLL.PLLN = 72;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 7;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK
| RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure the Systick interrupt time
*/
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq() / 1000);
/**Configure the Systick
*/
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
system_stm32f4xx.c (snippet)
#include "stm32f4xx.h"
#if !defined (HSE_VALUE)
#define HSE_VALUE ((uint32_t)8000000) /*!< Default value of the External oscillator in Hz */
#endif /* HSE_VALUE */
#if !defined (HSI_VALUE)
#define HSI_VALUE ((uint32_t)16000000) /*!< Value of the Internal oscillator in Hz*/ //DEFAULT 16000000
#endif /* HSI_VALUE */
stm32f4xx_hal_conf.h (snippet)
/* ########################## HSE/HSI Values adaptation ##################### */
/**
* @brief Adjust the value of External High Speed oscillator (HSE) used in your application.
* This value is used by the RCC HAL module to compute the system frequency
* (when HSE is used as system clock source, directly or through the PLL).
*/
#if !defined (HSE_VALUE)
#define HSE_VALUE ((uint32_t)8000000U) /*!< Value of the External oscillator in Hz */ //TEST 25000000) //DEFAULT: 8000000U
#endif /* HSE_VALUE */
#if !defined (HSE_STARTUP_TIMEOUT)
#define HSE_STARTUP_TIMEOUT ((uint32_t)100U) /*!< Time out for HSE start up, in ms */
#endif /* HSE_STARTUP_TIMEOUT */
/**
* @brief Internal High Speed oscillator (HSI) value.
* This value is used by the RCC HAL module to compute the system frequency
* (when HSI is used as system clock source, directly or through the PLL).
*/
#if !defined (HSI_VALUE)
#define HSI_VALUE ((uint32_t)16000000U) /*!< Value of the Internal oscillator in Hz*/ //DEFAULT: 16000000U
#endif /* HSI_VALUE */
2020-01-16 5:48 AM
The STM32 expects CMOS levels, not RS232 ones. Use a MAX3232 or equivalent.
Get a scope and check the baud rate by looking at the bit timing. Most GPS default to 9600 baud.
2020-01-16 6:44 AM
Thank you for your quick response!
The baudrate is stated in the datasheet of the GPS so it should be correct but I'll try to get a RS232 - CMOS Converter
Thanks a lot!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.