2025-09-22 11:41 AM
I want to use the SMT32N6 VFBGA142 or VFBGA169 package. These parts do NOT have XPSIM_P1(on port PO). They only have XPSIM_P2(on port PN).
Can I connect both Octo FLASH and Octo PSRAM on port PN and use the two chip selects (NCS1 & NCS2) to independently talk to the chips? I need to boot off the FLASH and then use the PSRAM to execute the program.
Any signal integrity issues or gotchas I need to keep in mind?
2025-09-23 1:42 AM
Both Flash and PSRAM must properly tri-state their outputs when not selected. Most modern Octo-SPI devices do this, but check the datasheets for both devices to confirm that when CS is not active, the outputs will be in high-Z state.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.