2025-06-05 4:32 AM - edited 2025-06-05 4:45 AM
Hi,
The example for FSBL works as described
But if the same approach is applied to Appli (Secure) code, the "User Setting Error" raised in DMA IRQ.
I use the XIP configuration.
Could you please elaborate chages to be made in Secure code?
Solved! Go to Solution.
2025-06-18 2:27 AM - edited 2025-06-18 9:15 AM
I am having the same issue with "User Setting Error" on GPDMA.
Edit: I found the root of my issue. I based my code off the example ADC_SingleConversion_TriggerTimer_DMA for the NUCLEO-N657X0-Q, instead of FSBL I used secure application. So if anyone else sees the same error this is the cause.
The problem is in two places.
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel0,DMA_CHANNEL_SEC|DMA_CHANNEL_NPRIV)!= HAL_OK )
{
Error_Handler();
}if you attach any peripheral (such as ADC) to the GPDMA in the application context you will see another call to this method in stm32n6xx_hal_msp.c HAL_ADC_MspInit
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel0, DMA_CHANNEL_PRIV|DMA_CHANNEL_SEC
|DMA_CHANNEL_SRC_SEC|DMA_CHANNEL_DEST_SEC) != HAL_OK)
{
Error_Handler();
}it gets called before the SystemIsolation_Config one. Commenting out the second one here fixes the first issue.
default_config.BaseAddress = __NON_CACHEABLE_SECTION_BEGIN;
default_config.LimitAddress = __NON_CACHEABLE_SECTION_END;does not work in the application context. The base and limit address is the same so if you use the __NON_CACHEABLE macros they do nothing. All you will see is zeroes at the memory addresses and the DMA user error. Changing the limit address to base address + your required buffer size allows the DMA to work.
2025-06-05 4:43 AM
Looks like I am not alone with this
2025-06-05 4:44 AM
BTW, I played with MPU regions, and even disabled the MPU at all. It had no effect.
2025-06-18 2:27 AM - edited 2025-06-18 9:15 AM
I am having the same issue with "User Setting Error" on GPDMA.
Edit: I found the root of my issue. I based my code off the example ADC_SingleConversion_TriggerTimer_DMA for the NUCLEO-N657X0-Q, instead of FSBL I used secure application. So if anyone else sees the same error this is the cause.
The problem is in two places.
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel0,DMA_CHANNEL_SEC|DMA_CHANNEL_NPRIV)!= HAL_OK )
{
Error_Handler();
}if you attach any peripheral (such as ADC) to the GPDMA in the application context you will see another call to this method in stm32n6xx_hal_msp.c HAL_ADC_MspInit
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel0, DMA_CHANNEL_PRIV|DMA_CHANNEL_SEC
|DMA_CHANNEL_SRC_SEC|DMA_CHANNEL_DEST_SEC) != HAL_OK)
{
Error_Handler();
}it gets called before the SystemIsolation_Config one. Commenting out the second one here fixes the first issue.
default_config.BaseAddress = __NON_CACHEABLE_SECTION_BEGIN;
default_config.LimitAddress = __NON_CACHEABLE_SECTION_END;does not work in the application context. The base and limit address is the same so if you use the __NON_CACHEABLE macros they do nothing. All you will see is zeroes at the memory addresses and the DMA user error. Changing the limit address to base address + your required buffer size allows the DMA to work.
2025-07-28 5:23 AM
Hi @neil1106
Thank you for your efforts!
The bullet #1 is exact.
Regarding item #2, the DMA buffer can reside in any memory region accessible by the DMA controller; however, cache clean or invalidate operations must be performed, depending on whether the CPU writes to or reads from that memory.
2025-09-23 1:23 AM
The reason
default_config.BaseAddress = __NON_CACHEABLE_SECTION_BEGIN; default_config.LimitAddress = __NON_CACHEABLE_SECTION_END;
does not work is the wrong definition of .noncacheable section in the linker file.
It should be the same as in FSBL project.
.noncacheable :
{
. = ALIGN(8);
__snoncacheable = .;/* create symbol for start of section */
KEEP(*(.noncacheable))
. = ALIGN(8);
__enoncacheable = .; /* create symbol for end of section */
} > RAM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.