2023-07-13 5:04 AM
Hello, I have a device that uses an STM32 microcontroller and has a USB port. I am attempting to create a secure access system for this device using a fingerprint module. My question is whether I can connect any fingerprint module to the device through the USB port and create a fingerprint lock system. Additionally, I am unsure about the process of connecting a fingerprint sensor to a device running a Real-Time Operating System (RTOS).
2023-07-20 6:45 AM - edited 2023-07-20 6:46 AM
Theoretically, yes, it is possible to connect a non-standard USB device by using the USB in host mode. However, you likely won't find a pre-build example of this and will have to implement the low level USB details yourself, provided those details are even available. It's not going to be as simple as installing drivers as you would do on a PC.
Note that "fingerprint device" is not a standard USB device like CDC, HID, or MSC.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.