2015-09-20 6:57 PM
how to configure GPIO PIN alternate function in hal driver ?
in std_periph driver i usually used this code: GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_TIM12); //TIM2_CH1 GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_TIM12); //TIM2_CH2 how to configure in Hal driver, can you help me about this code : // GPIO TypeDef Initialization GPIO_TypeDef GPIO_TypeDefStruct; /* // No se para que mierda es esto si uso PWM GPIO_TypeDefStruct.MODER |= ((31<<1)|(29<<1)|(27<<1)|(25<<1)); GPIO_TypeDefStruct.OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR15_1 | GPIO_OSPEEDER_OSPEEDR_14_1 GPIO_OSPEEDER_OSPEEDR13_1 | GPIO_OSPEEDER_OSPEEDR_12_1); */ GPIO_TypeDefStruct.AFR[1] |=(28<<GPIO_AF2_TIM4|24<<GPIO_AF2_TIM4|20<<GPIO_AF2_TIM4|16<<GPIO_AF2_TIM4); GPIO_TypeDef* GPIO_D = & GPIO_TypeDefStruct;2015-09-21 1:31 AM
Hi,
For example: Configuring USART3 Tx (PC10, mapped on AF7) as alternate function: GPIO_InitStruct.Pin = GPIO_PIN_10; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FAST; GPIO_InitStruct.Alternate = GPIO_AF7_USART3; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
2015-09-28 4:29 PM
thanx Edje, your information is very important for me. I also know it in stm32 cube example project, there are many configuration for all function of stm32. thanx edje hehehe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.