2015-09-30 5:34 AM
In my project based on stm32F107 i use four pins (PINE 12-15) to catch rising level on them.
My problem: two pins always produce external interrupts but there are no rising level on them and other two pins never respond to rising level.
My question: i'm looking for some debug ways and may be advices. May be reading some registers in the interrupt routine will help to solve my problem
Here is my code:RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOE, ENABLE);
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStruct.GPIO_Pin = GPIO_Pin_12; GPIO_Init(GPIOE, &GPIO_InitStruct); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_13; GPIO_Init(GPIOE, &GPIO_InitStruct); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_14; GPIO_Init(GPIOE, &GPIO_InitStruct); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_15; GPIO_Init(GPIOE, &GPIO_InitStruct); RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; // KeyI_0 GPIO_EXTILineConfig(GPIO_PortSourceGPIOE, GPIO_Pin_12); EXTI_InitStructure.EXTI_Line = EXTI_Line12; EXTI_Init(&EXTI_InitStructure); // KeyI_1 GPIO_EXTILineConfig(GPIO_PortSourceGPIOE, GPIO_Pin_13); EXTI_InitStructure.EXTI_Line = EXTI_Line13; EXTI_Init(&EXTI_InitStructure); // KeyI_2 GPIO_EXTILineConfig(GPIO_PortSourceGPIOE, GPIO_Pin_14); EXTI_InitStructure.EXTI_Line = EXTI_Line14; EXTI_Init(&EXTI_InitStructure); // KeyI_3 GPIO_EXTILineConfig(GPIO_PortSourceGPIOE, GPIO_Pin_15); EXTI_InitStructure.EXTI_Line = EXTI_Line15; EXTI_Init(&EXTI_InitStructure); NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_InitStructure.NVIC_IRQChannel = EXTI15_10_IRQn; NVIC_Init(&NVIC_InitStructure); void EXTI15_10_IRQHandler( void ) { printf( ''exti\n'' ); if (EXTI_GetFlagStatus(EXTI_Line12) != RESET) { EXTI_ClearITPendingBit(EXTI_Line12); printf( ''key1\n'' ); //keyboard_StringStart(0); } else if (EXTI_GetFlagStatus(EXTI_Line13) != RESET) { EXTI_ClearITPendingBit(EXTI_Line13); printf( ''key2\n'' ); //keyboard_StringStart(2); } else if (EXTI_GetFlagStatus(EXTI_Line14) != RESET) { EXTI_ClearITPendingBit(EXTI_Line14); printf( ''key3\n'' ); //keyboard_StringStart(3); } else if (EXTI_GetFlagStatus(EXTI_Line15) != RESET) { EXTI_ClearITPendingBit(EXTI_Line15); printf( ''key4\n'' ); //keyboard_StringStart(1); } } #exti #stm32f107
2015-09-30 5:55 AM
Are you sure you must configure the inputs as floating? Maybe you must pull them down or something?
2015-10-01 12:16 AM
So it was mistake in code syntax.
That is wrong:
GPIO_EXTILineConfig(GPIO_PortSourceGPIOE, GPIO_Pin_12);
That is correct:
GPIO_EXTILineConfig(GPIO_PortSourceGPIOE, GPIO_PinSource12);
Sorry for wasting your time.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.