2015-09-29 2:28 PM
I Trying To I2C Interface With DS1621 Using HAL Driver STM32Cube-MX 4.7.0
As Per HAL Driver I Try To Check Device Is Ready or NOT It Stuck At if(I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_SB, RESET, Timeout) != HAL_OK)It Always Getting timeout error what is the role ofI2C_FLAG_SB bit
&sharpdefine Slave_Address 0x90int main(void){ HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); //MX_I2C1_Init(); while (1) { MX_I2C1_Init(); if(HAL_I2C_IsDeviceReady(&hi2c1, Slave_Address, 10, 1000) == HAL_OK); if(HAL_I2C_Master_Transmit(&hi2c1, Slave_Address, ''0xEE'', 1, 1000) == HAL_OK); if(HAL_I2C_IsDeviceReady(&hi2c1, Slave_Address, 10, 1000) == HAL_OK); if(HAL_I2C_Master_Transmit(&hi2c1, Slave_Address, ''0xAA'', 1, 1000) == HAL_OK); if(HAL_I2C_IsDeviceReady(&hi2c1, 0x91, 10, 1000) == HAL_OK); if(HAL_I2C_Master_Receive(&hi2c1, 0x91, Temp, 2, 1000) == HAL_OK); }}void MX_I2C1_Init(void){ hi2c1.Instance = I2C1; hi2c1.Init.ClockSpeed = 100000; hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2; hi2c1.Init.OwnAddress1 = 64; hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLED; hi2c1.Init.OwnAddress2 = 0; hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_ENABLED; hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLED; HAL_I2C_Init(&hi2c1);}i used 1k resistor for pull-up what is the flow to use this driver please suggest me for initialization of I2C interfacealso suggest for tool where i can show signal activity #stm32f4-i2c-hal-driver #i2c-stm322015-09-30 10:31 PM
here is Standard Peripheral Used But still no data received please help me what thing i missed
#include ''main.h''uint32_t DS1621Timeout = DS1621_LONG_TIMEOUT;uint8_t DS1621_BufferRX[2] ={0,0};uint16_t tmp = 0, Add = 0;uint32_t DataNum = 0;uint16_t tempature = 0;void Delay(volatile int i){ for(volatile int y = 0; y <= 600; y++) { for(volatile int z = i; z<=100; z++); }} static void data_read(uint8_t DS1621_Add){ I2C_AcknowledgeConfig(DS1621_I2C, ENABLE); if((I2C_GetFlagStatus(DS1621_I2C, I2C_FLAG_RXNE)) == SET) { DS1621_BufferRX[0] = I2C_ReceiveData(DS1621_I2C); } I2C_AcknowledgeConfig(DS1621_I2C, DISABLE); I2C_GenerateSTOP(DS1621_I2C, ENABLE); if((I2C_GetFlagStatus(DS1621_I2C, I2C_FLAG_RXNE)) == SET) { DS1621_BufferRX[1] = I2C_ReceiveData(DS1621_I2C); } }static uint8_t data_write(uint8_t data){ I2C_SendData(DS1621_I2C, data); while((I2C_GetFlagStatus(DS1621_I2C, I2C_FLAG_TC)) == SET); return SUCCESS;}int main(void){ DS1621_Init(); DS1621_LowLevel_Init(); while (1) { if(DS1621_GetStatus() == SUCCESS) { Basic_Configuration(1, I2C_Direction_Transmitter); data_write(0xEE); data_write(0xAA); I2C_stop(I2C1); } if(DS1621_GetStatus() == SUCCESS) { Basic_Configuration(2, I2C_Direction_Receiver); data_read(DS1621_ADDR_R); I2C_stop(I2C1); } }}void DS1621_Init(void){ I2C_InitTypeDef I2C_InitStructure; I2C_DeInit(I2C1); I2C_SoftwareResetCmd(I2C1); /* DS1621_I2C configuration */ I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_AnalogFilter = I2C_AnalogFilter_Disable; I2C_InitStructure.I2C_DigitalFilter = 0x00; I2C_InitStructure.I2C_OwnAddress1 = 0x90; I2C_InitStructure.I2C_Ack = I2C_Ack_Disable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_Timing = 1000;//0x1045061D; /* Apply DS1621_I2C configuration after enabling it */ I2C_Init(DS1621_I2C, &I2C_InitStructure); /* DS1621_I2C Peripheral Enable */ I2C_Cmd(DS1621_I2C, ENABLE);}ErrorStatus DS1621_GetStatus(void){ uint32_t I2C_TimeOut = I2C_TIMEOUT; while(I2C_GetFlagStatus(DS1621_I2C, I2C_FLAG_BUSY)); /* Generate start */ I2C_GenerateSTART(DS1621_I2C, ENABLE); /* Wait until timeout elapsed */ while ((I2C_GetFlagStatus(DS1621_I2C, I2C_FLAG_BUSY) == SET) && (I2C_TimeOut-- != 0)); /* Check if Temp sensor is ready for use */ if ((I2C_GetFlagStatus(DS1621_I2C, I2C_ISR_NACKF) == RESET) || (I2C_TimeOut == 0)) { /* Clear NACKF and STOPF */ I2C_ClearFlag(DS1621_I2C, I2C_ICR_NACKCF | I2C_ICR_STOPCF); return ERROR; } else { /* Clear STOPF */ I2C_ClearFlag(DS1621_I2C, I2C_ICR_STOPCF); return SUCCESS; } }void DS1621_LowLevel_Init(void){ GPIO_InitTypeDef GPIO_InitStructure; /* DS1621_I2C Periph clock enable */ RCC_APB1PeriphClockCmd(DS1621_I2C_CLK, ENABLE); /* Configure the I2C clock source. The clock is derived from the HSI */ RCC_I2CCLKConfig(RCC_I2C1CLK_HSI); RCC_AHBPeriphClockCmd(DS1621_I2C_SCL_GPIO_CLK | DS1621_I2C_SDA_GPIO_CLK, ENABLE); /* Connect PXx to I2C_SCL */ GPIO_PinAFConfig(DS1621_I2C_SCL_GPIO_PORT, DS1621_I2C_SCL_SOURCE, DS1621_I2C_SCL_AF); /* Connect PXx to I2C_SDA */ GPIO_PinAFConfig(DS1621_I2C_SDA_GPIO_PORT, DS1621_I2C_SDA_SOURCE, DS1621_I2C_SDA_AF); /* Configure DS1621_I2C pins: SCL */ GPIO_InitStructure.GPIO_Pin = DS1621_I2C_SCL_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(DS1621_I2C_SCL_GPIO_PORT, &GPIO_InitStructure); /* Configure DS1621_I2C pins: SDA */ GPIO_InitStructure.GPIO_Pin = DS1621_I2C_SDA_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(DS1621_I2C_SDA_GPIO_PORT, &GPIO_InitStructure);}void DS1621_LowLevel_DeInit(void){ GPIO_InitTypeDef GPIO_InitStructure; /* Disable DS1621_I2C */ I2C_Cmd(DS1621_I2C, DISABLE); /* DeInitializes the DS1621_I2C */ I2C_DeInit(DS1621_I2C); /* DS1621_I2C Periph clock disable */ RCC_APB1PeriphClockCmd(DS1621_I2C_CLK, DISABLE); /* Configure DS1621_I2C pins: SCL */ GPIO_InitStructure.GPIO_Pin = DS1621_I2C_SCL_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(DS1621_I2C_SCL_GPIO_PORT, &GPIO_InitStructure); /* Configure DS1621_I2C pins: SDA */ GPIO_InitStructure.GPIO_Pin = DS1621_I2C_SDA_PIN; GPIO_Init(DS1621_I2C_SDA_GPIO_PORT, &GPIO_InitStructure);}void Basic_Configuration(uint8_t Data_Size, uint8_t I2C_Direction){ I2C_NumberOfBytesConfig(DS1621_I2C, Data_Size); if (I2C_Direction == I2C_Direction_Transmitter) { I2C_MasterRequestConfig(DS1621_I2C, I2C_Direction_Transmitter); I2C_SlaveAddressConfig(DS1621_I2C, DS1621_ADDR); } else { I2C_MasterRequestConfig(DS1621_I2C, I2C_Direction_Receiver); I2C_SlaveAddressConfig(DS1621_I2C, DS1621_ADDR_R); }}void I2C_stop(I2C_TypeDef* I2Cx){ // Send I2C1 STOP Condition I2C_GenerateSTOP(I2Cx, ENABLE);} #ifdef USE_FULL_ASSERTvoid assert_failed(uint8_t* file, uint32_t line){ while (1) { }}#endifWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.