2010-11-24 2:02 AM
STM32 : execute code from SRAM
2011-05-17 5:15 AM
''it does'nt work''
What, exactly, ''doesn't work''? In what way does it ''not work''?''help me please'' It's hard to help when you don't say what the actual problem is!2011-05-17 5:15 AM
2011-05-17 5:15 AM
Hi clive1,
What specific requirements?
2011-05-17 5:15 AM
There are specific requirements regarding the address used as a vector table location, and there will still need to be a primary vector table from which to boot.
You might need to modify your startup.s or crt0_gnu.s, to achieve your goals cleanly and efficiently.2011-05-17 5:15 AM
The alignment required by the NVIC unit.
You will need to copy the entire vector table into RAM, as well as the as having the one you booted from. The IRQ routines need to be in RAM, along with any library code it calls/touches. As any access to FLASH during the write/erase functions will block processor execution.2011-05-17 5:15 AM
I tried everything!
My vectors table is in SRAM, my IRQHandler is in SRAM and is executed when data arrives during the execution of FLASH_Erase but it is as if USART1 not working!I do not know what else to try!
This is myUSART1_ IRQHandler INRAM void INRAM_USART1_IRQHandler(void) { uint16_t reg; if ((USART1->SR & USART_FLAG_RXNE)) { // Réemission de la donnée USART1->DR = USART1->DR; Test=32; } if ((USART1->SR & USART_FLAG_IDLE)) { // Ligne IDLE // Clear IT pending reg = USART1->SR; reg = USART1->DR; IndexRcp = ID_ADR_DST; EnEcoute = TRUE; LgLSB = FALSE; } if ((USART1->SR & USART_FLAG_LBD)) { // LIN BREAK detection // Clear IT pending USART1->SR &= (uint16_t)~USART_FLAG_LBD; // La carte est transparente, le BREAK est envoyé immédiatement USART1->CR1 |= CR1_SBK_Set; Test=33; } if ((USART1->SR & USART_FLAG_ORE)) { // Error interrupt // OverRun Error interrupt UARTErreur |= USART_FLAG_ORE; reg = USART1->SR; reg = USART1->DR; } if ((USART1->SR & USART_FLAG_NE)) { // Noise Error interrupt UARTErreur |= USART_FLAG_NE; // Clear IT pending reg = USART1->SR; reg = USART1->DR; } }2011-05-17 5:15 AM
We'll I'm pretty sure that if you are executing ANY code from FLASH (ie outside your IRQ) it's going to be stalling the pipeline in a non-interruptable way.
The quickest way to test that is to make a small foot-print demo that runs completely in RAM.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.