2009-02-23 3:13 AM
STM32 - Burst read external NOR flash
2011-05-17 4:04 AM
STM32 (Access line, 512KB internal Flash, 48K Internal RAM)
My system's external flash memory reads have a timing constraint, and hence would like to use burst reads from a synchronous flash. Are there any app note or example source code of the processor configuration for burst reading an external flash in synchronous mode? How to set the number of half-words for the burst read. Thanks for any information.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.