2024-04-24 2:54 AM
Hi.. There
Recently i bought STEVAL-STWINKT1B kit with the WiFi adapter.
My motive is to connect the kit with the DSH-PREDMNT dashboard to run the FP-AI-PREDMNT2 demo
From my side, this is what i have done sofar
1. downloaded the FP-AI-PREDMNT2 firmware package
2. Installed the .bin file as it is what i found from the firmware package
3. Install the ST-BLE Sensor classic app with the phone and able to pair with the BLE
4. Made the account with the DSH-PREDMNT via default ST user credentials
5. Register the node via BLE APP with the DSH-PREDMNT dashboard
6. Added the WiFi credentials of one of my AP
However, everything goes well except WiFi connection!
Node never paired with the WiFi AP!
I never got the WiFi working with the default firmware!
I already got the JTAG debugger with the kit
To debug further more, i have forced the board in to the debug mode with the code!
but unfortunately, I'm not getting the debug logs at the serial terminal
How do i activate the debug logs ?
pl. suggest
Thanks
Mahendra
2024-06-25 7:12 AM
Hello,
checking with you on the solution, I still face the same issue and wasn't able to connect to the dashboard even though the device was recognized by the st-ble and was added to the cloud interface I got struck with wi-fi connection. let me know if you have solved this issue which will help me!
Best Regards
Dinesh Kumar
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.