2011-11-30 3:01 AM
Hello all,
I want to use the StdPeriph_Driver as a guide for my own project. Part: STM32F100RB value line discovery (test kit). Trying to get the I2C to work. I want to use the I2C files (.c+.h) for my own project. So when I put these files in my own project (included correctly I think: I put the files i2c.c and i2c.h in de src folder and included - stm32f10x.h and - stm32f10x_conf.h in the firmware folder and included in the i2c.h file like: &sharpinclude ''../firmware/stm32f10x.h'' &sharpinclude ''../firmware/stm32f10x_conf.h'' Now I call the I2C_StructInit function in my main.c But it gives the error: too few arguments to function 'I2C_StructInit' I've absolutely no idea what to include in that function. i2c.c void I2C_StructInit(I2C_InitTypeDef* I2C_InitStruct){ ... } I2C_InitTypeDef refers to: typedef struct{ ... declaring variables. }I2C_InitTypeDef; If a take a look at void I2C_Init(I2C_TypeDef* I2Cx, I2C_InitTypeDef* I2C_InitStruct){ ... } Then I see that I2Cx need to be I2C2 (the I2C I use). But what does I2C_InitStruct need to be?your help
is very appreciated
! If I do something wrong here, just mention it. Greets, Dennis. #stm32l-discovery-i2c-problem #i2c2011-11-30 6:33 AM
Show your code that is failing, everyone has the library.
You would normally point to the library/include code by telling the compiler where there directories are, or drop them in the project. For most of the project templates it's a matter of uncommenting line is stm32f10x_conf.h to pull in the right peripherals. { I2C_InitTypeDef I2C_InitStructure; I2C_Cmd(I2C2, ENABLE); I2C_StructInit(&I2C_InitStructure); I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = SLAVE_ADDRESS7; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = ClockSpeed; I2C_Init(I2C2, &I2C_InitStructure); ..2011-11-30 7:20 AM
Find my problem.
ST gives you the option to create your own memory location for the I2C_InitTypeDef struct. I didn't knew what to do with it, but now I know. In the i2c.c file I wrote: static I2C_InitTypeDef I2C_InitStruct; For creating a memory location for the struct. now I've done this, it works, I'm not getting errors from it anymore. But I've absolutely no idea why they created a InitStruct to fill in the struct of the I2C registers. I should only use the Init function to write to these registers. Or am I wrong and is this usefull after all? Greets, Dennis.2011-11-30 8:07 AM
It is a temporary structure feed to the library routines to configure the hardware. Once done it is never used again. I wouldn't make it a static/global structure.
It often makes sense to use the I2C_StructInit() to clear the structure to default settings, especially when allocated from the stack as a local variable. Remember the stack contains random junk when the local variables are not explicitly set/initialized. You could program the I2C peripheral registers directly, but then you'd need to deal with a whole level of minutia that becomes very unportable across device families.2012-06-26 11:09 PM
Hi All;
I am using STM32L Discovery board to do I2C write and read to M24C64 eeprom via I2C interrupt. When I continous writing the EEPROM (with about 10mS interval), I find it lost data. From the Scope, a bad packet is only a START, no ''7 bits of address'', no Slave address and no data pulse. Attached is the source code and read me.txt file. Any solution? Regards Samuel ________________ Attachments : STM32_I2C_WR_Via_Int.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzoN&d=%2Fa%2F0X0000000bQY%2Fa1k9yF5tyCGm3.BJSfnsoi6mqyzeYGmrtWqttNxpxys&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.