2018-03-22 5:36 AM
Hi, I am trying to download SWO stream from ST32f746 discovery board. I was able to see all of the ouptut in 'Printf via SWO Viewer' .
I want to have binary values to be dumped. Is it possible to download this by ST-LINK_CLI.exe or other way?
I could not find any way to solve this problem in 'ST-LINK Utility UM.pdf' or command line help.Thanks
2018-03-22 7:25 AM
It is just a stream of bytes, not sure if available software creates a means to export to a file, etc.
ITM_SendChar() doesn't care if it is ASCII data, or bytes from a variable or structure. The ITM interface is quite wide, you could arguable send data in different ways, but you'd have to own a lot more of the interface, drivers, etc.
Consider using the USART-VCP attached to the ST-LINK, at high baud rates, and export to your favorite terminal or logging application.
ST had a memory viewer tool. Keil can SAVE data from memory to a file, perhaps use the SDRAM as a logging buffer, then save data to file.
2018-03-22 11:51 AM
'Consider using the USART-VCP attached to the ST-LINK, at high baud rates, and export to your favorite terminal or logging application.'
There is SB16 which is connection between MCU TRACESWO pin and ST-LINK in UM1907 manual. I can unsolder it and use USART-VCP to download data to my fav terminal, but I cannot understand how attaching USART-VCP to ST-Link (STLINK_TX-PA2 and STLINK_TR-PA3 pins - Figure 22. ST-LINK/V2-1 with support of SWD only ) can work. Could you explain? ThanksWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.