STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407G-DISC1 board - USAR2 baud not correct

Posted on March 22, 2018 at 17:51I have a STM32F407G-DISC1 eval board that I'm trying to connect to my 'Linux' laptop using USART2 on the eval board and a prolific RS232<->USB converter attached to my laptop. Using the STM32CubeMX 4.25 software I ge...

What is the maximum STM32F7 TIM1 PWM frequency?

Posted on March 22, 2018 at 16:02Now I am using STM32F7 Discovery board. I want to make TIM1 PWM with high frequency.I made 10MHz PWM frequency. However, I can't increase the PWM frequency even though I change 'Prescaler ' and 'Period '.htim1.Init.P...

choies1 by Associate
  • 2813 Views
  • 2 replies
  • 0 kudos

CubeMx Generates Garbage Init Code??

Posted on March 16, 2018 at 02:05Using CubeMX V4.7.1 I get garbage initialization code for RTC.c when I request initialization be generated as .c.h file pairs.Simple demo case:Start CubeMXNew ProjectSelect STMf103C8Tx as targetUnder Pins Select RTC-...

In ping-pong code of STM32L072 Discovery kit LoRa module, can we enable Radio Receive interrupt and use it instead of polling it using Radio.Rx in the main loop? At present the ping-pong code does polling in main while(1) loop, I want it to be interrupt b

Posted on March 22, 2018 at 11:09At present the Pin-pong code polls for the data received on Radio(RF), can we use Radio Receive interrupt in place of Radio.Rx() function?#radio-receive-interrupt

F103 ADC DMA - help ! a question

Posted on March 19, 2018 at 16:55hello dear forum,I want use ADC + DMA with F103I want start ADC conversion with external input and want ADC convert 50 samples and stop until next starthowever with every start ADC measures one single sample and put ...

['F446 header] incorrect comments

Posted on January 03, 2018 at 16:30In [STM32Cube_FW_F4_V1.18.0]\Drivers\CMSIS\Device\ST\STM32F4xx\Include\stm32f446xx.h :#define SAI_xFRCR_FRL              SAI_xFRCR_FRL_Msk                           /*!<FRL[1:0](Frame length)  */should be#define SA...

RSA sign

Posted on April 22, 2016 at 11:59Hi i have a problem with RSA signing. when i use RSA_PKCS1v15_Verify  function from ST library, i get a error of rsa Invalid Key.is there any function that i can create a modulus?.. 

arunease by Associate II
  • 1559 Views
  • 3 replies
  • 0 kudos

Resolved! CRH support missing in stm32f1xx_ll_gpio.h ?

Posted on March 05, 2018 at 20:48Using TrueStudio for STM32 v.9.0.0  and STMCubeMX v.4.24.0STM32F100C8 and Low Layer drivers.I noticed that LL support for GPIO ports above GPIO_PIN_7 does not work. I tried to use GPIO_PIN_13 on GPIOC but saw that PI...

Willunen by Associate III
  • 2502 Views
  • 6 replies
  • 0 kudos

Older versions of the STM32 PMSM MC Library

Posted on March 22, 2018 at 10:03Hi,Is it possible to get hold of earlier versions of the STM32 PMSM MC Library?I have inherited an older project, and are trying to 'dis-entangle' the project-specific changes from the pristine library source.The spe...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.