2018-04-11 1:52 AM
ST-Link CLI rease another sector.
STM32F767ZI, dual bank.
When using the commandline-switch -SE 15 st-link cli (v 3.2.0.0) reports:
ST-LINK Firmware version : V2J29S7
Connected via SWD.SWD Frequency = 4000K.Target voltage = 2.8 V.Connection mode : Normal.Device ID:0x451Device flash Size : 2048 KbytesDevice family :STM32F76xMemory Sector @0x0810C000 erasedbut erased sector 0x08108000.
Version 2.5.0 reports:
ST-LINK Firmware version : V2J29S7
Connected via SWD.SWD Frequency = 4000K.Target voltage = 2.8 V.Connection mode : Normal.Device ID:0x451Device flash Size : 4095 KbytesDevice family :STM32F76xMemory Sector @0x0810C000 is not erased. Verify the memory protection.Bank2 erase can resolve this problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.